Hello , i am using code warrior 5.9 which run on XP only, i want to use latest code warrior 10.1 (on windows 7) so how to migrate is question?
I got 1 PDF online which explains about creating xml file for configuration but i am not confident that i am going on correct path for migration.
sanjyot kadu
The latest CodeWarrior for MCU is v10.5, which can be downloaded from:
To import a Classic CodeWarrior to Eclipse CW, user needs to create a new bareboard project in CW10.5 and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application not for how to do this:
http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf
But if you are using DSC products, CodeWarrior v10.5 includes CodeWarrior Classic Project Importer for CW DSC v8.3 projects.
For how to do it, please refer to section 3.8 in CW10.5 Targeting Manual:
C:\Freescale\CW MCU v10.5\MCU\Help\PDF\Targeting_Microcontrollers.pdf