I am planning to use IMX6 for a 4 channel analog video (D1 size) capture, save and upload to network in JPEG format. i will use one TVP5158 for four of the analog cameras and obtain an interleaved parellel video data (16 bit) connected to one CSI port of IMX. Does IMX CSI module can "de-interleave" four video streams, if so, how it is done?
Thank you
Ayhan
The CSI port it is connected to the VDIC ( Video De-Interlacer) I think I am not quite understanding if the four videos are in the same buffer and only need to de-interleave this buffer. because it is only one at time.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------