MAG3110 Stop Working When After Switch Off And On

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAG3110 Stop Working When After Switch Off And On

608 Views
eranoren
Contributor I

Hi all,

I'm using a MAG3110 on a board quite similar to the TI Sensortag, a cc2541 controlling the MAG via I2C, but without all other sensors (just the mag).

I would like to use the MAG only once in a while (say, every 10 minutes for a few seconds, to save battery), so I'm using the 20miliamp pins of the TI to control the power in and out of the MAG.

I manage to get results from the MAG up to the first shut down, after that it seems that the measurement stops. When I'm giving a continuous "1" signal through that pin I keep getting measurements.

What could be the problem?

Thank you very much in advance,

Eran

Tags (1)
0 Kudos
2 Replies

373 Views
Joshevelle
Senior Contributor I

Hello Eran,

Is the IIC bus still active while you "turn off" the MAG3110?

Please take a look at the datasheet page 6, table 4, Absolute Maximum Ratings:

http://cache.freescale.com/files/sensors/doc/data_sheet/MAG3110.pdf

Input voltage on any control pin (SCL, SDA) --> -0.3 to VDDIO + 0.3

If the IIC bus is still active while VDDIO is a zero logic, unknown behavior might occur or even worst, permanent damage.  Instead of suppress the supply voltage, I would rather recommend you to set the device status to STANDBY mode by setting the SYSMOD register (0x08) to 0x00.

In  STANDBY mode the MAG3110 would only draw ~2uA.

Hope it helps!

Josh

0 Kudos

373 Views
Martin35804
NXP Employee
NXP Employee

Hi,

please consider following:

Where to post a Discussion?

0 Kudos