AnsweredAssumed Answered

imx6q: FEC ENET: rcv is not +last

Question asked by Prasant J on Feb 27, 2014
Latest reply on Mar 19, 2015 by Oliver Graute

Hi All,

 

I'm using linux release 3.0.35_4.0.0 on my custom hardware (design based on sabre sd platform). I'm using Micrel's Gigabit Ethernet PHY KSZ9021RNI.

 

When connected to a 100 mbps network, my network is stable. But when I connect to a 1000 mbps link, network is very unstable. The ssh connection freezes or breaks.

On the terminal log I can see: net eth0: FEC ENET: rcv is not +last

 

I tried the linux kernel from 3.0.35_4.1.0 release (not the UBoot, only the kernel) but I was still getting the problem.

 

 

Can anyone throw light on this issue ?

As I understand that this was a known issue and was solved in the later releases. Is that is true: what was the exact problem ?

 

 

Any inputs will of help to me. Thanks!

 

 

-Pj

Outcomes