AnsweredAssumed Answered

MX6Q-SDP problem with keyboard

Question asked by Xiaoqiang Yang on Feb 23, 2014
Latest reply on Mar 3, 2014 by Xiaoqiang Yang

Hi all,

 

I am using MX6Q-SDP connectted with USB mouse,keyboard and LVDS.After linux run,the touch screen and usb mouse can

work well, but the keyboard can't work.And I got some error after boot up:

 

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

(EE) XKB: No components provided for device Virtual core keyboard

unrecognised device identifier!

(EE) config/hal: NewInputDeviceRequest failed (2)

matchbox: keyboard does not appear to have a &1

if ; then

IS_BABBAGE=YES

Xfbdev -keybd keyboard,,device=/dev/input/keyboard0 -mouse mouse,2,device=/dev/input/mice &

fi

 

if ; then

Xfbdev -mouse tslib,2,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&

else

Xfbdev -mouse mouse,2,device=/dev/input/mice&

fi

 

sleep 8

 

matchbox-window-manager -d -use_lowlight no -use_titlebar yes -use_cursor yes&

matchbox-desktop&

matchbox-panel  --bgtrans yes  &

sleep 5

  1. Calibrate when using the rootfs the first time

  2. Check whether the touch screen exists

if ; then

ls /usr/etc | grep pointercal > /dev/null 2>&1

if ; then

  ts_calibrate

fi

fi

 

Thanks in advance!

 

Outcomes