Hello Jim,
Thank you verry mush for your effort!
I have change the settings of the prm file just you sayd. I change "INTO ROM" to 0x4000 and I comment out the _Startup and without converting the s19 file I can download it to the CARDS12.
When the _Startup is not comment out than the monitor program gives an write error at FFE0.
I have try to add the code the mentioned but the compiler promt that tIsrFunc is not declare.
But I'm happy that I can download the s19 file generated by CW.
There two question:
1) after downloading into the CARDS12 I run the program on 0x4000 (syntax for
TwinPeek = g4000) then the led beginns to blink. But if I type g8000 the led is blinking to so the code is programmed on two memory locations??
2) I have comment out the _Startup entry in the prm file what is the purpose of this entry and when do I need it?
Thanx!