iMX6sl Kernel support HS200?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6sl Kernel support HS200?

849 Views
admin
Specialist II

Hi Sir,

I get kernel source code from git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx

and i check out the source code from tag jb4.3_1.0.0-ga.

I read the source code, i found its not support eMMC HS200 tuning(but support SD UHS1),

where can i get the patch of support HS200?

Thanks!!

with Best Regards,

Quccc

Tags (3)
0 Kudos
1 Reply

483 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi CCC,

Mx6sl can support eMMC4.5 working on HS200 mode. We've verified Toshiba, Samsung eMMC4.5 worked well on HS200 on mx6sl evk for L3.10.17 release.Before L3.10 release, eMMC4.5 can not work on HS200 for imx6sl since the SW does not support it.

Towards the patch you refer to, I have not seen it anywhere. Hope this can help you~~

Have a great day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos