console IO interrupt uart5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

console IO interrupt uart5

Jump to solution
563 Views
Catosh
Contributor IV

Helllo,

currently I am using a TWM k60 evm module.

I would like to use the console IO component trough UART5, and I would like to be able to enable interrupts on this component.

Anyway, using ProcessorExpert, I am not able to change "Interrupt/service event" value into enable because it is disabled.

I previously enabled CPU's NMI.

I suppose is "obvious" not enabling interrupts on port used as debug purpose, but I am not sure.

Any hint would be gladly appreciated.

Best regards,

Luca.

0 Kudos
1 Solution
391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Luca,

    Yes, you are right, the console IO component  is really can't set the the interrupt function, because it is the integrated component.

    If you want to use the interruption, you can choose the "Serial_LDD" component, "AsynchroSerial" component or "Init_UART" component, these components can set the interrupts.

    You just choose wrong component.

    Wish my answer will help you!

    If you still have question, please let me know!

Best regards!

Jingjing

View solution in original post

0 Kudos
1 Reply
392 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Luca,

    Yes, you are right, the console IO component  is really can't set the the interrupt function, because it is the integrated component.

    If you want to use the interruption, you can choose the "Serial_LDD" component, "AsynchroSerial" component or "Init_UART" component, these components can set the interrupts.

    You just choose wrong component.

    Wish my answer will help you!

    If you still have question, please let me know!

Best regards!

Jingjing

0 Kudos