Hi, please check with your local sales office for detailed plans regarding kernel upgrades.
Any updates on this? Does Freescale intend to provide a later 3.10.x kernel with the android jb 4.3 or 4.4 releases? It seems power management is much better in the later kernels (compared to 3.0.35_4.1.0). I am getting the following errors on my custom board running jb4.3
BUG: soft lockup - CPU#1 stuck for 22s! [kinteractiveup:1358]
Modules linked in:
Pid: 1358, comm: kinteractiveup
CPU: 1 Not tainted (3.0.35-gde33f0b-dirty #7)
PC is at generic_exec_single+0x6c/0x90
LR is at arch_send_call_function_single_ipi+0x34/0x38
pc : [<c00bfba0>] lr : [<c0052c4c>] psr: 200e0013
sp : d6b6fe28 ip : 00000000 fp : c0a267d0
r10: 00000001 r9 : c14568c8 r8 : 01411000
r7 : c14568c0 r6 : 00000000 r5 : c14568c0 r4 : d6b6fe54
r3 : 00000001 r2 : f2a01000 r1 : 00000005 r0 : c0700a0c
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 236c404a DAC: 00000015