AnsweredAssumed Answered

I have 10 Kinetis parts,  mark M04R5VLF, 1N96F, CTGYQDD,   doing strange things..   I thou they were MKL04Z32VLF4's  but can't figure it out from the data sheat, as to what there realy are, can any one help ?

Question asked by Lachlan Audas on Feb 4, 2014
Latest reply on Feb 6, 2014 by Santiago Gonzalez Fabian

I have 10 Kinetis parts,  mark M04R5VLF, 1N96F, CTGYQDD,   doing strange things, are there MKL04Z32VLF'S ?

 

Debugging works fine..   but can't get any output pin's to change, or even driven,   also the Reset pin is oscillating,  around 700 Hz,   but,,   the debugger works just fine,

and status shows no Reset, but for the Debugger reset,   I can program flash..  etc..  just fine,  programer appears to run fine too.. but no pin outputs on any pin..

 

Lachlan

Outcomes