AnsweredAssumed Answered

Window 7 64-bit Host driver for USB OTG port for 'SABRE for Automotive Infotainment Based on the i.MX 6 Series' evaluation board

Question asked by Steven Cao on Feb 4, 2014
Latest reply on Mar 31, 2014 by Yixing Kong

I have a 'SABRE for Automotive Infotainment Based on the i.MX 6 Series' evaluation board.

My onboard CPU is IMX6U which is i.MX 6DualLite processor.

I have successfully built U-boot and Linux Kernel.


I am using the USB OTG port (on CPU board) to work as a USB CDC ACM serial port. On my Ubuntu 12.04, I can communicate with the target as a serial port when USB cable was connected.

 

However, I could not get my Windows 7 64-bit PC to work with it, Window 7 failed to find a correct driver. I googled the internet and did not find a good one for it.

 

Do you have a Window 7 64-bit USB CDC AMC serial driver  and INF file that you can send to me? It should be a generic driver for all USB CDC ACM.

 

Thanks,

 

Steven

Outcomes