AnsweredAssumed Answered

Micron 1GB RAM with iMX6

Question asked by Vasan V S on Jan 31, 2014
Latest reply on Jan 31, 2017 by Jithin M

Hi all,

 

We are trying to use Micron 1GB RAM module with an iMX6 based system that we are building.

 

The DDR calibration for the Micron 1GB DDR3 RAM with the Part number MT41J128M16HA-15E is available with the current code base. The specifications of this part is Clock rate 667MHz, Data Rate 1333 MHz and CL as 9.


However, we are trying to use another part number MT41K128M16JT-125 XIT (Micron 1GB DDR3 RAM) with the Clock rate of 800 Mhz, Data rate of 1600Mhz and CL as 11. When we run the image with the setting of the older part number with slower clock rate, we get unexplained kernel crashes.


Is there anybody who has integrated the newer Micron 1GB RAM with this partnumber successfully with iMX6?


Thanks in advance to all your inputs.


Vasan


Outcomes