AnsweredAssumed Answered

need Mictor connector test board for IMX6SL EVK board

Question asked by danmez on Jan 23, 2014

I need to develop a small test circuit and connect to some GPIO on the IMX6SL EVK development board.  The signals I need to use are on the Mictor connector on the EVK.

 

Can someone recommend a small test board that is available off the shelf?  Ideally it would have the mating Mictor connector on one side and bring the signals to some larger connector or header so I can make easy connections.  If it had a little proto board that would be nice as well.

 

Thanks!

Outcomes