Hi,
I am using CMake for developing the Makefile, I have also
created tool chain file for the same, but it is not working as per expectation.
Any one has developed toolchain file or used CMake 2.8 for Codewarrior? It
would be helpful if some experts can share experiences on CMake and code
warrior
I have not used CMake to generate makefile for Qorivva,but you can try to configure its build tool chains as the command line tools in CodeWarrior.
For Classic CodeWarrior, these tools are under:
<CW path>\CW for MPC55xx and MPC56xx 2.x\PowerPC_EABI_Tools\Command_Line_Tools
For Eclipse CodeWarrior, they are under:
<CW path>\CW MCU v10.x\MCU\PA_Tools\Command_Line_Tools