I need to deploy it to multiple systems in a lab environment. Licensing is being done via FlexLM
.
I used to be able to install 6.3 using the /S /V"/passive" switches, but this will not work anymore.
If someone could point me in the right direction or web link it would be appreciated, I have had no success searching the web or Freescale.
Thanks
CW10.5 also support silent install (/S /D=c:\Freescale\CW MCU v10.5).
we can download CW6.3 special edition from this link:
http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS
CW10.3 is no longer available on freescale website. please use CW10.5 from above link if you want to use eclipse version.
does this answer your quesion?
Sorry, I'm not after the older version of Codewarrior, I only want to know if there are a specific set of command line switches that can be used with setup.exe that will enable a full silent installation of MCU 10.x
thanks