AnsweredAssumed Answered

Build ltib error......

Question asked by sangjin hong on Jan 21, 2014
Latest reply on Jan 22, 2014 by Rita Wang

I'm sure that I was successful to build ltib for i.MX 6 previous week.

 

I don't know why???

Please help me !!!

 

However, I tried to build ltib this monday, but I couldn't do that.

There was build error.

 

I referenced i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf document.

I ran the following commands:

 

$ tar zxvf L3.0.35_4.1.0_130816_source.tar.gz

$ ./L3.0.35_4.1.0_130816_source/install

$ cd <LTIB directory>

$ ./ltib -m config

 

 

there was a error like the following:

 

*****************************************************************************************************************************

$ ./ltib -m config

Installing host support packages.

 

This only needs to be done once per host, but may take up to

an hour to complete ...

 

If an error occurs, a log file with the full output may be found in:

/home/istech/dev/freescale/dev_env/ltib/host_config.log

 

Exiting on error or interrupt

Please see >> /home/istech/dev/freescale/dev_env/ltib/host_config.log for details

*****************************************************************************************************************************

 

host_config is like the following:

 

*****************************************************************************************************************************

Processing platform: Host support packages

============================================

using /home/istech/dev/freescale/dev_env/ltib/config/platform/host/ltib.preconfig

 

Processing: fake-provides

===========================

 

Processing: mkspooflinks

==========================

 

Processing: distcc

====================

 

Processing: ccache

====================

 

Processing: m4

================

 

Processing: bison

===================

 

Processing: flex

==================

Build path taken because: directory build, no prebuilt rpm,

 

Cowardly refusing to clobber existing directory:

/opt/freescale/ltib/usr/src/rpm/BUILD/flex-2.5.37

Remove this by hand if you really want to rebuild this package from scratch

 

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

*****************************************************************************************************************************

Outcomes