SRTC of i.MX51 is not Enabled at cold start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRTC of i.MX51 is not Enabled at cold start

1,827 Views
yuuki
Senior Contributor II

I have a problem that SRTC is not Enabled at cold start.

I checked the status register. It seems that SRTC has shifted to the Failure state, because it detected some alarms.

LPSR (Status Reg) = 0x00000065

- EAD bit = 1: Security alarm detected

- TR bit = 1: Counter has reached its maximum value

- CTD bit = 1: Clock Tampering Detected.

- TRI bit = 1: Time read is invalidated.

LPGR (General Purpose Reg) = 0x82400000

- SW_ISO = 1: SRTC is isolated from the rest of the SoC.

Is it able to be enabled when SRTC is in a Failure state?

Best Regards,

Tags (2)
0 Kudos
13 Replies

1,544 Views
yuuki
Senior Contributor II

Dear Yixing-san,

Thank you for your reply.

This problem has not been solved yet.
However, our customer gave up about this problem.
For that reason, I will close this discussion.

Best Regards,

0 Kudos

1,544 Views
yuuki
Senior Contributor II

Hi, Weisong Liu-san,

Thank you for your reply.

> 1, does the SRTC work properly when you re-initiate the SRTC atfer cold power-on?
=>
There is a case where the SRTC does not work properly.
"1" cannot be set to EN_LP gas bit of a LPCR register.
And 0x41736166 value cannot be written to LPPDR register.
(in this case, Value of LPPDR register is 0x4944c5a8)

> 2, when the issue occurs, what's the SRTC time? the data is reseted to "0"?
=>
LPSCMR and LPSCLR register are 0x00000000.

Please advise of your findings.

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

please enclose the schmetic of power section for i.mx51 here.

thanks

0 Kudos

1,544 Views
yuuki
Senior Contributor II

Dear Weisong Liu-san,

Thank you for your reply.

I am sorry, I cannot enclose a schmetic here.
Is there any method of sending it only to you?

Best Regards,

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

please send to b19830@freescale.com, I will review it and send feedback here.

0 Kudos

1,544 Views
yuuki
Senior Contributor II

Dear Weisong Liu-san,

Thank you for your reply.

I send the schematic of a power section to you.
Would you check this?

Best Regards,

0 Kudos

1,544 Views
YixingKong
Senior Contributor IV

Yuuki

Has your question been answered, or do you need help form SW team?

Regards,

Yixing

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

if you make sure RTC_1V2 and 32k input of i.mx51 are good in off mode.

we may need help from software AE.

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

I saw the schematic.

you have ensured that RTC_1V2 is ok when powering off, right?

so do you also please check if CLK32KMCU is connected to 32K input of i.mx51 and enabled in MC13892 in off mode?

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

I saw the schematic.

you have ensured that RTC_1V2 is ok when powering off, right?

so do you also please check if CLK32KMCU is connected to 32K input of i.mx51 and enabled in MC13892 in off mode?

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

how do you supply NVCC_SRTC? is it a coin cell when powering off?

0 Kudos

1,544 Views
yuuki
Senior Contributor II

Dear Weisong Liu-san,

Thank you for your reply.

As for NVCC_SRTC, 1.2V is supplied when powering off.

0 Kudos

1,544 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Yuuki

a few questions:

1, does the SRTC work properly when you re-initiate the SRTC atfer cold power-on?

2, when the issue occurs, what's the SRTC time? the data is reseted to "0"?

0 Kudos