Hello,Jiao,
We provide MFG Tools to cusotmer for burning android images and linux images into SD card and Flash on board. Did you try to use it ? As for android RF, you can refer to mx6 sabreSD board and create a new RF for cusotmer board. when you run "source build.....", the customized board can be included, then lunch it.
Regards,
Weidong
Last time I checked, the MFG Tools requires me to connect the board, so I assume it only works for Freescale reference board, am I wrong? What are the steps to use it to burn Android image to any SD card?
Can I lunch for sabreSD and then use the generated RF plus my own Android kernel? In case some modifications are needed, which file I need to look at? Hope you can provide some directions for me as I'm very to Android porting.
For this particular question: "What are the steps to use it to burn Android image to any SD card?" You can use the script ' fsl-sdcard-partition.sh' located on the source tarball. This way, you do not need the MFGtool, just a Linux host with the SD card.