AnsweredAssumed Answered

FFS Mutex problem.

Question asked by Daniel Chai on Jan 15, 2014

Hi All,

 

Now I installed the FFS patch on MQX4.0.2 on TWRK60F120M.

And I installed the wear leveling without installing MFS on NAND FLASH.

When I try to use read/write NAND FLASH in a interrupt, it prints: "assertion failed: 0, file simple_mutex.cpp, line 141".

After digging into it, I found it can not lock the mutex because it can lock the mutex in a interrupt.

 

Do anyone have any ideas how can use read/write based on FFS in a interrupt?

 

 

Thank you.

 

-Daniel

Outcomes