iMX6D DDR3 Fly-by Termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6D DDR3 Fly-by Termination

Jump to solution
2,252 Views
sithara
Contributor II

In my application, i have two DDR3( 2x 1Gbx16) interfaced to iMX6D. Fly by topology is used for better SI. Any freescale recommendation for parallel termination resistor value ? Does series termination required for DDR3 interface of iMX6D? If so, what is the optimum value?

Labels (2)
0 Kudos
1 Solution
1,308 Views
Yuri
NXP Employee
NXP Employee

You may try the fly-by for 2 parts, using general recommendations of 

Chapter 3 (i.MX 6 Series Layout Recommendations) in "Hardware Development Guide

for i.MX 6 ...". Next, simulation should be provided to define termination resistors.  


Also, let me remind, DDR calibration must be provided for such topology.

"i.MX 6 Series DDR Calibration"

< http://cache.freescale.com/files/32bit/doc/app_note/AN4467.pdf >

View solution in original post

0 Kudos
5 Replies
1,308 Views
Yuri
NXP Employee
NXP Employee

   According to the i.MX6 Design Checklist, it is suggested to use "T" topology

when the number of DDR3 chips are not more than four. Otherwise "Fly-by"

Topology is recommended, since it allows to decrease timing / trace length

requirements because of additional calibration procedures.

0 Kudos
1,308 Views
sithara
Contributor II

Is there any issue when i use Fly by topology for 2 DDR3 ? I have checked hardware user guide and design checklist of iMX6D. Nowhere it is mentioned fly-by is not recommended for less than 2 chips.

Also, i have seen that DDR3 is built for Fly-by routing...

0 Kudos
1,309 Views
Yuri
NXP Employee
NXP Employee

You may try the fly-by for 2 parts, using general recommendations of 

Chapter 3 (i.MX 6 Series Layout Recommendations) in "Hardware Development Guide

for i.MX 6 ...". Next, simulation should be provided to define termination resistors.  


Also, let me remind, DDR calibration must be provided for such topology.

"i.MX 6 Series DDR Calibration"

< http://cache.freescale.com/files/32bit/doc/app_note/AN4467.pdf >

0 Kudos
1,308 Views
sithara
Contributor II

Is there any recommendations for the resistor values when i opt fly-by?

0 Kudos
1,307 Views
Yuri
NXP Employee
NXP Employee

Please look at the enclosed.