I find a bug about USBDM4.10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I find a bug about USBDM4.10.6

420 Views
wangbaode
Contributor IV

Hi pgo,

I think I find a bug about USBDM4.10.6. I install USBDM 4.10.6 and codewarrior6.3 on my computer.

I want to debug MC9S08FL16 throutgh USBDM in codewarrior6.3.when I new a project,I just find HCS08 FSL open souce BDM.

because My hardware is based-on JS16,I can't debug FL16 with my BDM.

pastedImage_0.png

But,I uninstall the USBM4.10.6 and install USBDM4.9.4. I can find HcS08 open source BDM.

pastedImage_0.png

so I think it's a bug.

best regards for you

bye

Tags (2)
0 Kudos
1 Reply

253 Views
pgo
Senior Contributor V

Hi Wang,

Definitely a bug.

The HCS08 Open Source BDM is considered obsolete by Freescale so more recent devices don't have that as an option e.g. MC9S08FL16 though similar chips such as the MC9S08FL8 does.

USBDM is meant to patch the XML files in Codewarrior to add in the missing option.  It appears to be currently broken with the merge program throwing an exception.  I have located the problem and (I hope) fixed it. This fix will appear in the next version.

bye

0 Kudos