AnsweredAssumed Answered

MQX RTCS demos

Question asked by Pato Three on Jan 10, 2014
Latest reply on Jan 14, 2014 by Pato Three

Running bare-metal on the TWRVF65GS10 with DS-5, most of the MQX 4.0.2 examples are running fine, however for the RTCS eth_to_serial demo, it goes up to "Waiting for  incoming connection..." and then just sits there. IP is configured manually on WIN7 and HyperTerminal returns: "Unable to connect to 192.168.1.202: port 23" and it's the same result with either A5 or M4.

 

When running httpsrv, I can ping to itself but not to the PC.

 

Also I followed the "General Technical MQX FAQ" guidelines.

 

Has anyone managed to get those demos to work on the VF6 without modifications ? with modifications ?

 

Many thanks in advance

Outcomes