AnsweredAssumed Answered

iwl4965 firmware

Question asked by Xiaoqiang Yang on Jan 10, 2014
Latest reply on Nov 24, 2014 by kenny wang

Hi everyone,

 

I placed a iwl4965 into the mini pcie slot and power on my MX6Q SABRE SD board.After I entered linux,

I can find it by 'lspci':

root@linaro-ubuntu-desktop:~# lspci

00:00.0 PCI bridge: Device 16c3:abcd (rev 01)

01:00.0 Network controller: Intel Corporation PRO/Wireless 4965 AG or AGN  Network Connection (rev 61)

But it seems not to work,when I type 'ifconfig',it shows:

root@linaro-ubuntu-desktop:~# ifconfig

eth0      Link encap:Ethernet  HWaddr 00:04:9f:02:cd:2e

          inet addr:192.168.2.115  Bcast:192.168.2.255  Mask:255.255.255.0

          UP BROADCAST RUNNING MULTICAST  MTU:576  Metric:1

          RX packets:24 errors:0 dropped:0 overruns:0 frame:0

          TX packets:31 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:4245 (4.2 KB)  TX bytes:4400 (4.4 KB)

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

And during start up,I found some related Information--->

............

fec_enet_mii_bus: probed

iwl4965: Intel(R) Wireless WiFi 4965 driver for Linux, in-tree:

iwl4965: Copyright(c) 2003-2011 Intel Corporation

PCI: enabling device 0000:01:00.0 (0140 -> 0142)

iwl4965 0000:01:00.0: Detected Intel(R) Wireless WiFi Link 4965AGN, REV=0x4

iwl4965 0000:01:00.0: device EEPROM VER=0x36, CALIB=0x5

iwl4965 0000:01:00.0: Tunable channels: 13 802.11bg, 4 802.11a channels

IMX-PCIe: MSI 0x3f01 @0x0:0x1ff8000, irq = 497

.............

.............

iwl4965 0000:01:00.0: request for firmware file 'iwlwifi-4965-2.ucode' failed.

iwl4965 0000:01:00.0: no suitable firmware found!

.............

 

Where can I find its firmware? How to use?

 

Thanks in advance!

 

 

Xiaoqiang

 

Outcomes