MX6Q SABRESD nfs boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6Q SABRESD nfs boot

Jump to solution
906 Views
xiaoqiangyang
Contributor III

Hi everyone,

I selected my profile > Minimum bootable root filesystem ,and selected root filesystem image type>ext2.gz ramdisk.

After buiding completed,I boot my board via nfs.It ran to a state that I haven't know:

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Linux version 3.0.35-2666-gbdde708 (yxq@bruce) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #6 SMP PREEMPT Tue Jan 7 11:37:37 CST 2014

CPU: ARMv7 Processor revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Ignoring unrecognised tag 0x54410008

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 194560

Kernel command line: console=ttymxc0,115200 root=/dev/nfs ip=dhcp nfsroot=192.168.2.130:/srv/rootfs,v3,tcp video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=sin1

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 512MB 256MB = 768MB total

Memory: 765660k/765660k available, 282916k reserved, 0K highmem

Virtual kernel memory layout:

vector : 0xffff0000 - 0xffff1000 ( 4 kB)

fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

DMA : 0xf4600000 - 0xffe00000 ( 184 MB)

vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)

lowmem : 0x80000000 - 0xc0000000 (1024 MB)

pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

.init : 0x80008000 - 0x8003c000 ( 208 kB)

.text : 0x8003c000 - 0x80aa71b0 (10669 kB)

.data : 0x80aa8000 - 0x80b0d540 ( 406 kB)

.bss : 0x80b0d564 - 0x80b5b4ac ( 312 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

bio: create slab <bio-0> at 0

mxs-dma mxs-dma-apbh: initialized

print_constraints: SPKVDD: 4200 mV

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1

mc_pfuze 1-0008: FAB: 0 ,FIN: 0

print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV

print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV

print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV

print_constraints: PFUZE100_VREFDDR: at 750 mV

print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV

print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV

print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

max17135 2-0048: PMIC MAX17135 for eInk display

i2c-core: driver using legacy suspend method

i2c-core: driver using legacy resume method

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

PMU: registered new PMU device of type 0

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = c0880000 suspend_iram_base=c091c000

PM driver module loaded

IMX usb wakeup probe

add wake up source irq 75

IMX usb wakeup probe

cpu regulator mode:ldo_bypass

regulatorget: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 1495

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

regulatorget: get() with no identifier

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb

mxc_ldb mxc_ldb: for second ldb displdb mode should in separate mode

mxc_sdc_fb mxc_sdc_fb.1: NO mxc display driver found!

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd

mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb

mxc_ldb mxc_ldb: for second ldb displdb mode should in separate mode

mxc_sdc_fb mxc_sdc_fb.3: NO mxc display driver found!

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console enabled, bootconsole disabled

console enabled, bootconsole disabled

loop: module loaded

No sata disk.

m25p80 spi0.0: found m25p32, expected sst25vf016b

m25p80 spi0.0: m25p32 (4096 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000100000 : "bootloader"

0x000000100000-0x000000400000 : "kernel"

GPMI NAND driver registered. (IMX)

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1

egalax_ts 1-0004: egalax_ts: failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

input: eGalax Touch Screen as /devices/platform/imx-i2c.2/i2c-2/2-0004/input/input2

elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

input: isl29023 light sensor as /devices/virtual/input/input3

isl29023 2-0044: driver version 1.0 enabled

i2c-core: driver using legacy suspend method

i2c-core: driver using legacy resume method

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19

mag3110 2-000e: check mag3110 chip ID

input: mag3110 as /devices/virtual/input/input4

mag3110 2-000e: mag3110 is probed

i2c-core: driver using legacy suspend method

i2c-core: driver using legacy resume method

input: mma845x as /devices/virtual/input/input5

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform using DMA

mmc1: SDHCI controller on platform using DMA

mmc2: SDHCI controller on platform using DMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

Galcore version 4.6.9.6622

Thermal calibration data is 0x5764de7d

Thermal sensor with ratio = 180

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usbcore: registered new interface driver snd-usb-audio

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver using legacy suspend method

i2c-core: driver using legacy resume method

imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.

wm8962 0-001a: customer id 0 revision D

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 SEM08G 7.39 GiB

mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB

mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB

mmcblk0: p1

mmcblk0boot1: unknown partition table

mmcblk0boot0: unknown partition table

input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input6

asoc: wm8962 <-> imx-ssi.1 mapping ok

input: wm8962-audio DMIC as /devices/platform/soc-audio.5/sound/card0/input7

input: wm8962-audio Ext Spk as /devices/platform/soc-audio.5/sound/card0/input8

imx_3stack asoc driver

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

#0: wm8962-audio

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

eth0: Freescale FEC PHY driver (mii_bus:phy_addr=1:01, irq=-1)

mmc2: new high speed SDHC card at address e624

mmcblk1: mmc2:e624 SU16G 14.8 GiB

mmcblk1: p1

PHY: 1:01 - Link is Up - 100/Full

Sending DHCP requests ., OK

IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.2.108

IP-Config: Complete:

device=eth0, addr=192.168.2.108, mask=255.255.255.0, gw=192.168.2.10,

host=192.168.2.108, domain=, nis-domain=(none),

bootserver=0.0.0.0, rootserver=192.168.2.130, rootpath=, mtu=576

VFS: Mounted root (nfs filesystem) on device 0:12.

Freeing init memory: 208K

sh-2.05b#

I can't use linux command like 'ls',but when I press Tab,it displayed some commands:

sh-2.05b#

Display all 108 possibilities? (y or n)

! command exit kobs-ng return trap

. compgen export let root true

.matchbox complete false lib sbin type

: continue fc local select typeset

[ declare fg logout set udevinfo

[[ dev fi mnt sh udevtest

]] dirs for opt shift ulimit

alias disown function perf shopt umask

bash do getopts popd smtpd.py unalias

bashbug done hash printf source unit_tests

bg echo help proc startx unset

bin elif history pushd suspend until

bind else home pwd sys usr

boot enable idle pydoc test var

break esac if python then wait

builtin etc in python2.4 time while

case eval jobs read times {

cd exec kill readonly tmp }

I is normal? Or how can I fix it?

Thanks in advance!

0 Kudos
1 Solution
486 Views
LeonardoSandova
Specialist I

you need to install busybox, it has all these basic Unix commands. Also, pressing TAB, it activates auto-completion, and because it is an empty string, it will print all binaries under those directories on PATH

Leo

View solution in original post

0 Kudos
1 Reply
487 Views
LeonardoSandova
Specialist I

you need to install busybox, it has all these basic Unix commands. Also, pressing TAB, it activates auto-completion, and because it is an empty string, it will print all binaries under those directories on PATH

Leo

0 Kudos