Writing in DDR is inverted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing in DDR is inverted

Jump to solution
1,225 Views
kpanchamia
Contributor I

Hi,

I have a strange problem with DDR.

Project specs:

Kinetis k61FX512

DDR part : MT46V16M16

Using the DDR init script provided in the sample. I have adapted it for DDR and above mentioned part.

I have written a temp function as:

{

  volatile uint8_t * u8ptrTmp = (uint8_t *) 0x080000F0;

  volatile uint8_t u8Tmp;

  volatile uint8_t u8TmpBuff[10];

  for(u8Tmp = 0 ; u8Tmp < 10 ; u8Tmp++)

  {

  u8ptrTmp[u8Tmp] = u8Tmp;

  }

  for(u8Tmp = 0 ; u8Tmp < 10 ; u8Tmp++)

  {

  u8TmpBuff[u8Tmp] = u8ptrTmp[u8Tmp];

  }

  for(;;);

}

Objective is to write 10 bytes starting at 0x08000000 & reading them back in a buffer.

The writing happens but very oddly, like:

0x080000F0 = 0x07

0x080000F1 = 0x06

0x080000F2 = 0x05

0x080000F3 = 0x04

0x080000F4 = 0x03

0x080000F5 = 0x02

0x080000F6 = 0x01

0x080000F7 = 0x00

And reading happens properly as in buffer shows 0x07, 0x06....0x00.

Tried changing endianness, but no luck. It results in

0x080000F0 = 0x04

0x080000F1 = 0x05

0x080000F2 = 0x06

0x080000F3 = 0x07

0x080000F4 = 0x00

0x080000F5 = 0x01

0x080000F6 = 0x02

0x080000F7 = 0x03

DDR config code:

void ext_ddr_init(void)

{

  /* Enable DDR controller clock */

  SIM_SCGC3 |= SIM_SCGC3_DDR_MASK;

  /* Enable DDR pads and set slew rate */

  //SIM_MCR |= 0xC4;   // bits were left out of the manual so there isn't a macro right now

  SIM_MCR |= 0x64; // For DDR instead of DDR2

  DDR_RCR |= DDR_RCR_RST_MASK; // Force software reset

  //* (vuint32 *)(0x400Ae1ac) = 0x01030203;

  * (vuint32 *)(0x400Ae1ac) = 0x00000003; // Since ODT is absent in DDR config

  //DDR_CR00 = 0x00000400;    // DDRCLS = 4 is reserved??

  DDR_CR00 = 0x00000000; //For selecting DDR Class

  u32Temp = DDR_CR01; //DDR_CR01 is read only. Gives Maxcol = 11, Max row = 0x10 & CS = 2

  //DDR_CR02 = 0x02000031; // Init time & refresh count

  DDR_CR02 = 0x0F00FFFF;

  //DDR_CR03 = 0x02020506;

  DDR_CR03 = 0x1F010506; // delay, 1 for ddr

  //DDR_CR04 = 0x06090202;

  DDR_CR04 = 0xFF3F0707;

  //DDR_CR05 = 0x02020302;

  DDR_CR05 = 0x1F070F0F;

  //DDR_CR06 = 0x02904002;

  DDR_CR06 = 0x009040FF;

  //DDR_CR07 = 0x01000303;

  DDR_CR07 = 0x01010303;

  //DDR_CR08 = 0x05030201;

  DDR_CR08 = 0x1F1FFF01;

  //DDR_CR09 = 0x020000c8;

  DDR_CR09 = 0x02000FFF;

  DDR_CR10 = 0x03003207;

  DDR_CR11 = 0x01000000;

  DDR_CR12 = 0x04920031;

  DDR_CR13 = 0x00000005;

  DDR_CR14 = 0x00C80002;

  DDR_CR15 = 0x00000032; //  | DDR_CR15_SREF_MASK ;

  DDR_CR16 = 0x00000001;

  DDR_CR20 = 0x00030300;

  DDR_CR21 = 0x00040232;

  DDR_CR22 = 0x00000000;

  DDR_CR23 = 0x00040302;

  DDR_CR25 = 0x0A010201;

  //DDR_CR25 = 0x0A020200;

  DDR_CR26 = 0x0101FFFF;

  DDR_CR27 = 0x01010101;

  DDR_CR28 = 0x00000003;

  DDR_CR29 = 0x00000000;

  DDR_CR30 = 0x00000001;

  //DDR_CR34 = 0x02020101;

  DDR_CR34 = 0x00000000;

  DDR_CR36 = 0x01010201;

  DDR_CR37 = 0x00000200;

  DDR_CR38 = 0x00200000;

  DDR_CR39 = 0x01010020;

  DDR_CR40 = 0x00002000;

  DDR_CR41 = 0x01010020;

  DDR_CR42 = 0x00002000;

  DDR_CR43 = 0x01010020;

  DDR_CR44 = 0x00000000;

  DDR_CR45 = 0x03030303;

  DDR_CR46 = 0x02006401;

  DDR_CR47 = 0x01020202;

  DDR_CR48 = 0x01010064;

  DDR_CR49 = 0x00020101;

  DDR_CR50 = 0x00000064;

  DDR_CR52 = 0x02000602;

  DDR_CR53 = 0x03c80000;

  DDR_CR54 = 0x03c803c8;

  DDR_CR55 = 0x03c803c8;

  DDR_CR56 = 0x020303c8;

  DDR_CR57 = 0x01010002;

  asm("NOP");

  DDR_CR00 |= 0x00000001;

  while ((DDR_CR30 & 0x400) != 0x400);

  MCM_CR |= MCM_CR_DDRSIZE(0);   

}

Attached are images of the same


I need to transfer & run code from DDR at bootup. So I need to be able to write & read sequentially byte by byte.


Kindly suggest if anymore details are required.


Thanks...

0 Kudos
1 Solution
711 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Thank you for the patience.

Please download K70 DDR memory initialization tool from below link, which provide DDR1 memory example about related register setting.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K70_120&nodeId=01624698C9DE2DDDB1&fps...

Wish it helps.

View solution in original post

0 Kudos
4 Replies
711 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Besides of hardware connection issue, I think most caused by DDR controller registers setting.

Please check below pictures about TWR-K70F120M board DDR2 registers setting.

Wish it helps.

DDR1.jpg

DDR2.jpg

711 Views
kpanchamia
Contributor I

Hi, thanx for replying.

Already tried with the tower config and all sorts of register combinations (well most of them), but no luck

Can you send across or point to some code or sample of K60/K61/K70 interfaced with DDR1 RAM and not DDR2.

Or does freescale have any evaluation board containing Kinetis and DDR 1 RAM??

Thank You

0 Kudos
712 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Thank you for the patience.

Please download K70 DDR memory initialization tool from below link, which provide DDR1 memory example about related register setting.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K70_120&nodeId=01624698C9DE2DDDB1&fps...

Wish it helps.

0 Kudos
711 Views
kpanchamia
Contributor I

Awesome !!

Working now. Used the tool. Thanks a lot !!

0 Kudos