Hi
Is USB Control Register (USBC0_CTRL) address a 0x4003_5800 or 0x4003_4800?
It is written as USB Control Register (USBC0_CTRL) :0x4003_5800 in VYBRIDRM.pdf/2143page.
But, It is USB Control Register (USBC0_CTRL):0x4003_4800 in IAR EWARM.
Best regards,
soichi
Solved! Go to Solution.
0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.
0x40034800 seems working properly. Table 3-2 Peripheral bridge 0 slot assignment tells that 0x4003_4000 slot is used for USBC0 and 0x4003_5000 slot is not used.
Dear TIC team,
Is mention of VYBRIDRM.pdf/2143page an error in writing of Manual?
If it is an error of Manual, please revise Manual.
Best Regards,
soichi
Thanks for your help, kef!
Soichi,
I marked this typo in the Reference Manual to fix it in the next revision. - Thanks for finding it!
Sincerely, Naoum Gitnik.
Dear Edward,
Thank you for reply.
Sorry,
Best Regards,
soichi