AnsweredAssumed Answered

RTCS network bind error with a static IP and netmask other than 255.255.255.0

Question asked by Travis Long on Dec 19, 2013
Latest reply on Dec 20, 2013 by Travis Long

I'm working with a MK60DN512 project which uses RTCS Ethernet.  Everything works great when using DHCP, and works great when using a static IP address with a netmask of 255.255.255.0.  As soon as I change the 4th byte of the netmask to anything other than zero, I get a network bind error when it attempts to bind (error 4 is returned).  Has anyone else experienced this, and if so, what can be done to overcome it?

 

Forgot to mention I am using MQX version 3.8 on this particular project.

 

Thanks in advance!

Outcomes