Hello,
I'm trying to connect an external EEPROM via SPI to a MPC5554. At the document "Qorivva Simple Cookbook “Hello World” Programs to Exercise Common Features on MPC5500 & MPC5600 Microcontrollers" I found an example code to perform a single transfer from DSPI_C to DSPI_D. This programm works very fine. But now I want to replace the DSPI_D on the MPC5554 with an external EEPROM.
Here is the code from the example with my ideas:
// no changes, because the master on the MPC5554 still sets the system clock
void initSysclk (void) {
FMPLL.SYNCR.R = 0x16080000;
while (FMPLL.SYNSR.B.LOCK != 1) {};
FMPLL.SYNCR.R = 0x16000000;
}
// also no changes, because DSPI_C is the master
void initDSPI_C(void) {
DSPI_C.MCR.R = 0x80010001; /* Configure DSPI_C as master */
DSPI_C.CTAR[0].R = 0x780A7727; /* Configure CTAR0 */
DSPI_C.MCR.B.HALT = 0x0; /* Exit HALT mode: go from STOPPED to RUNNING state*/
SIU.PCR[107].R = 0x0A00; /* MPC555x: Config pad as DSPI_C SOUT output */
SIU.PCR[108].R = 0x0900; /* MPC555x: Config pad as DSPI_C SIN input */
SIU.PCR[109].R = 0x0A00; /* MPC555x: Config pad as DSPI_C SCK output */
SIU.PCR[110].R = 0x0A00; /* MPC555x: Config pad as DSPI_C PCS0 output */
}
void initDSPI_D(void) {
// delete this funktion, because the external EEPROM just need hardwire signals SOUT, SIN, SCK and PCS0 from master
}
void ReadDataDSPI_D(void) {
// no ideas how to read from the slave
}
void ReadDataDSPI_C(void) {
// no ideas how to read from the slave
}
int main(void) {
initSysclk();
initDSPI_C();
initDSPI_D();
DSPI_D.PUSHR.R = 0x00001234;
DSPI_C.PUSHR.R = 0x08015678;
ReadDataDSPI_D(); /* Read data on slave DSPI */
ReadDataDSPI_C(); /* Read data on master DSPI */
while (1) {i++; } /* Wait forever */
}
It would be nice, if someone could help me.
Thanks and best regards
Flo
Hi,
Unfortunately this is so general question to be able to help directly.
You did not specify the EEPROM type/part number.
According to AC characteristics stated within its datasheet you will have to set CTAR properly.
Also the datasheet describes READ and WRITE sequences and instructions used for that.
Based on this you will know what commands should be pushed into PUSHR register and what you will read back from POPR.
Regards,
Petr