Hi everyone,
I need to test some GUI, so I need to connect the device to a video.
I was able to let it work booting from SD with these parameters in u-boot
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait video=mxcfb0:dev=hdmi,1920x1200M@60,if=RGB24
I've tried putting the video part in bootargs_nfs, but it isn't working. I've read in another post that in NFS the HDMI device became mxcfb1, but hadn't luck with ith either.
Any hints?
Thanks
MIX
Hi Massimo,
When you built BSP in LTIB , the Target Image Generation you need to chose "NFS ONLY". It means that the uImage you download to your board is the one generated under NFS Target image.
Hope this can help you~~
Best Regards
Dan