AnsweredAssumed Answered

i.MX6Q Watchdog Question

Question asked by Paul DeMetrotion on Dec 11, 2013
Latest reply on Oct 28, 2014 by Anson Huang

I have a Linux BSP that was built with a custom board file that includes the following line which should load the watchdog timer.

    

 

     imx6q_add_imx2_wdt(0, NULL);

 

During boot I get the following console message.

 

     imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

 

Problem is the timer is not enabled and has not loaded 60s into the timer. Does the WD timer start automatically or does it need to be manually started? I do have the following device available- /dev/watchdog.

Outcomes