AnsweredAssumed Answered

Has someone succeeds booting android from NFS?

Question asked by Yamil Garcia on Dec 11, 2013

I'm trying to boot a custom board from NFS with no success, it get stucked when init memory is freed.

I fallowed the intructions from Android_User_Guide.pdf. I don't see any error output.

Can someone give a hint on this issue?

 

I attached the log file to show command line, etc.

 

....

ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Sending DHCP requests ., OK

IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.38

IP-Config: Complete:

     device=eth0, addr=192.168.1.38, mask=255.255.255.0, gw=192.168.1.1,

     host=192.168.1.38, domain=imagikcorp.local, nis-domain=(none),

     bootserver=0.0.0.0, rootserver=192.168.1.35, rootpath=

VFS: Mounted root (nfs filesystem) on device 0:12.

Freeing init memory: 236K

Original Attachment has been moved to: android_log.txt.zip

Outcomes