Hi,all
I use LTIB L2.6.35_10.12.01 to build package openswan-2.6.18
I want to run ipsec protocol in iMX28 platform,but in the process of running openswan i got a problem and need help:
When i excute ipsec setup start,openswan needs about 5~7 minutes to create a connection,it's so slowly and very strange.
Why the openswan need a lot of time to create a ipsec connection?
I use two virtual machines run centOS5, compile openswan-2.6.18 with same sourece to test,but it create a connection very fast
So i compile newer version of openswan to test,i try version 2.6.26 and 2.6.38 and get same problem
P.S I use wireshark to capture packets
Does anyone can give me some suggestion or solution?