Fellow engineers,
I am working with an p4080 based board. I am trying to get 2 PCIE controllers probed properly.
In uboot I have no problems scanning and discovering what is connected to both controllers/PCI bridges.
For both PCIE1/2 uboot sets up the Primary, secondary and Subordinate bus numbers to 0,1,1 respectively.
When linux boots up and probes the controllers, PCIE1 is probed and the bridge scanned properly but PCIE2 is probed at the bridge but not attempted a scan.
I see this message
"pci 0001:02:00.0: bridge configuration invalid ([bus 01-01]), reconfiguring
"
I updated uboot to set the secondary and subordinate numbers to 2 (left the primary number to 0) and a subsequent kernel boot scanned the bus for PCIE2 successfully.
I found these numbers to be very critical since the device tree blob (bus-range) for pci is also based off these.
I'd like to get a good fix rather than the uboot hack and get better understanding of the problem. If there are any pointers someone could provide it would be awesome.
Thank you
Hi Ruchika,
I am also facing the same problem.
In mine, pci-1 is not detecting the device(sata controller), bcz of sata controller problem.
pci-2 is detecting the device(xr17v35x uart controller) in the uboot. And when booting the kernel i am seeing the exact message that u see.
"pci 0001:02:00.0: Primary bus is hard wired to 0
pci 0001:02:00.0: bridge configuration invalid ([bus 01-01]), reconfiguring"
After kernel booted, the driver is loading successfully.But an attempt to read/write to the devices make the kernel crash
root@p1023:~# echo 123 > /dev/ttyXR0
Machine check in kernel mode.
Caused by (from MCSR=10008): Bus - Read Data Bus Error
Oops: Machine check, sig: 7 [#1]
P1023 RDB
After that i updated the uboot(in pciauto_postscan_setup_bridge() to secondary and subordinate bus number to 2), since it is fixed the bridge reconfiguring issue for u.
Now uboot is detecting the device as before while it is booting. But when i list it via command "pci 2 long", I am not seeing the device and checked the "pci 1 long' that second and subordinate bus numbers are 2. But subsequent kernel boot now shows as below, and hence i am seeing the same kernel crash, when an attempt to read/write to the device.
"pci 0001:02:00.0: Primary bus is hard wired to 0
pci 0001:02:00.0: bridge configuration invalid ([bus 02-02]), reconfiguring"
So, can you plz let me know exactly what u changed in the uboot and/or dts file to fix this issue.?
Thanking you
S.Sivakumar
Which version SDK are you using?
Would you please provide the whole u-boot and Kernel boot up log(without your modification)? We will do more investigation.
Hi,
We have fixed the issue here.
We had mapped the PCIe2 in the 36 bit memory space. But the driver(exar xr17v35x) expects the device to be within the 32bit memory space.
Then we changed it back, only the PCIe2 to be within the 32bit space in the uboot/law and dts file.. This is working now(crashing is not happening)
Thanks for the support
I am using freescale SDK 1.4 / kernel 3.8.13.
Thanks & Regards,
S.Sivakumar
I am facing same problem with PCIE driver in new Linux kernel
shipped along with SDK-V1.5-20131219 .I was using old
kernel Linux version 3.0.48 previously and now updated to
Linux version 3.8.13-rt9 inorder to add IEEE1588 support in
Eatherner driver . After updating to the new kernel ,the device
drivers are not woring properly and i am getting some error
messages in the boot-up . Please find below bootlog snippet
for both old kernel (PCIe working ) and the new one (PCIe not
working )
Working old kernel(linux version 3.0.48)
===============================
PCIe1: disabled
PCIe2: Root Complex, x1, regs @ 0xfe201000
01:00.0 - 13a8:0358 - Simple comm. controller
PCIe2: Bus 00 - 01
PCIe3: disabled
In: serial
Out: serial
Err: serial
SERDES bank 1 reference clock: 100MHz
SERDES bank 2 reference clock: 100MHz
Net: Initializing Fman
Fman1: Uploading microcode version 106.1.4
Change supported feature to 100:FD/HD for addr 6 features(X) 28C
FM1@DTSEC1 connected to Broadcom BCM54616S, address 6
Fiber optic mode active
FM1@DTSEC2 connected to Broadcom BCM54616S, address 7
Change supported feature to 100:FD/HD for addr 12 features(X) 28C
FM1@DTSEC3 connected to Broadcom BCM54616S, address 12
Fiber optic mode active
FM1@DTSEC4 connected to Broadcom BCM54616S, address 9
FM1@DTSEC5 connected to Broadcom BCM54616S, address 10
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5
Hit any key to stop autoboot: 0
=> boot
Setting bus to 1
Error writing the chip.
NAND read: device 0 offset 0x100000, size 0x500000
5242880 bytes read: OK
NAND read: device 0 offset 0x600000, size 0x100000
1048576 bytes read: OK
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-3.0.48-rt70
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3972344 Bytes = 3.8 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0x00c00000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03fe5000, end 03fff1a9 ... OK
WARNING: could not find compatible node fsl-usb2-mph or fsl-usb2-dr: FDT_ERR_NOTFOUND.
Using P2041 RDB machine description
Memory CAM mapping: 256/256/256/256 Mb, residual: 0Mb
Linux version 3.0.48-rt70 (root@localhost.localdomain) (gcc version 4.6.2 (GCC) ) #138 SMP PREEMPT RT Fri May 30 17:51:01 IST 2014
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000200000)
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000001000000)
Qman ver:0a01,01,02
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000)
Bman ver:0a02,01,00
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc(0x0000000001000000)
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc(0x0000000000a00000)
No USDPAA memory, no 'usdpaa_mem' bootarg
CPU maps initialized for 1 thread per core
bootconsole [udbg0] enabled
Found FSL PCI host bridge at 0x0000000ffe201000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe201000 ranges:
MEM 0x0000000c20000000..0x0000000c3fffffff -> 0x00000000e0000000
IO 0x0000000ff8010000..0x0000000ff801ffff -> 0x0000000000000000
/pcie@ffe201000: PCICSRBAR @ 0xdf000000
P2041 RDB board from Freescale Semiconductor
Zone PFN ranges:
DMA 0x00000000 -> 0x00040000
Normal empty
Movable zone start PFN for each node
early_node_map[1] active PFN ranges
0: 0x00000000 -> 0x00040000
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 10 pages/cpu @b1083000 s18752 r8192 d14016 u40960
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: root=/dev/mtdblock4 rootfstype=jffs2 rw console=ttyS0,115200
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 969004k/1048576k available (7824k kernel code, 79572k reserved, 280k data, 553k bss, 276k init)
Kernel virtual memory layout:
* 0xfffdf000..0xfffff000 : fixmap
* 0xfdfe9000..0xfe000000 : early ioremap
* 0xf1000000..0xfdfe9000 : vmalloc & ioremap
Preemptible hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 4 CPUs
mpic: ISU size: 256, shift: 8, mask: ff
mpic: Initializing for 256 sources
clocksource: timebase mult[efffffb] shift[22] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
mpic: requesting IPIs...
e500 family performance monitor hardware support registered
Brought up 4 CPUs
devtmpfs: initialized
xor: measuring software checksum speed
8regs : 760.000 MB/sec
8regs_prefetch: 660.000 MB/sec
32regs : 784.000 MB/sec
32regs_prefetch: 677.000 MB/sec
xor: using function: 32regs (784.000 MB/sec)
NET: Registered protocol family 16
EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe201000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 493 for PCI Err
MPC85xx_edac PCI err registered
PCI: Probing PCI hardware
pci 0000:00:00.0: ignoring class b20 (doesn't match header type 01)
PCIE error(s) detected
pci 0000:00:00.0: PCI bridge to [bus 01-ff]
PCIE ERR_DR register: 0x80020000
PCIE ERR_CAP_STAT register: 0x80000001
PCIE ERR_CAP_R0 register: 0x00000800
PCIE ERR_CAP_R1 register: 0x00000000
PCIE ERR_CAP_R2 register: 0x00000000
PCIE ERR_CAP_R3 register: 0x00000000
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io 0xfdfea000-0xfdff9fff]
pci 0000:00:00.0: bridge window [mem 0xc20000000-0xc3fffffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
bio: create slab <bio-0> at 0
raid6: int32x1 62 MB/s
raid6: int32x2 112 MB/s
raid6: int32x4 189 MB/s
raid6: int32x8 166 MB/s
raid6: using algorithm int32x4 (189 MB/s)
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Not working new kernel(linux version 3.8.13)
===============================
PCIe1: disabled
PCIe2: Root Complex, x1, regs @ 0xfe201000
01:00.0 - 13a8:0358 - Simple comm. controller
PCIe2: Bus 00 - 01
PCIe3: disabled
In: serial
Out: serial
Err: serial
SERDES bank 1 reference clock: 100MHz
SERDES bank 2 reference clock: 100MHz
Net: Initializing Fman
Fman1: Uploading microcode version 106.1.4
Change supported feature to 100:FD/HD for addr 6 features(X) 28C
FM1@DTSEC1 connected to Broadcom BCM54616S, address 6
Fiber optic mode active
FM1@DTSEC2 connected to Broadcom BCM54616S, address 7
Change supported feature to 100:FD/HD for addr 12 features(X) 28C
FM1@DTSEC3 connected to Broadcom BCM54616S, address 12
Fiber optic mode active
FM1@DTSEC4 connected to Broadcom BCM54616S, address 9
FM1@DTSEC5 connected to Broadcom BCM54616S, address 10
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5
Hit any key to stop autoboot: 0
Setting bus to 1
Error writing the chip.
NAND read: device 0 offset 0x100000, size 0x500000
5242880 bytes read: OK
NAND read: device 0 offset 0x600000, size 0x100000
1048576 bytes read: OK
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-3.8.13-rt9
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 4542147 Bytes = 4.3 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0x00c00000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03fe5000, end 03fff1a9 ... OK
WARNING: could not find compatible node fsl-usb2-mph or fsl-usb2-dr: FDT_ERR_NOTFOUND.
Using P2041 RDB machine description
Memory CAM mapping: 256/256/256/256 Mb, residual: 0Mb
Linux version 3.8.13-rt9 (root@localhost.localdomain) (gcc version 4.7.3 (GCC) ) #7 SMP PREEMPT RT Wed Aug 6 13:16:30 IST 201 4
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000200000)
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000002000000)
Qman ver:0a01,01,02
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000)
Bman ver:0a02,01,00
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc(0x0000000001000000)
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc(0x0000000000a00000)
No USDPAA memory, no 'usdpaa_mem' bootarg
CPU maps initialized for 1 thread per core
setup_arch: bootmem
arch: exit
bootconsole [udbg0] enabled
P2041 RDB board from Freescale Semiconductor
Zone ranges:
DMA [mem 0x00000000-0x3fffffff]
Normal empty
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x00000000-0x3fffffff]
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 8 pages/cpu @b11de000 s10752 r8192 d13824 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: root=/dev/mtdblock4 rootfstype=jffs2 rw console=ttyS0,115200
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 885312k/1048576k available (9156k kernel code, 163264k reserved, 340k data, 552k bss, 268k init)
Kernel virtual memory layout:
* 0xfffdf000..0xfffff000 : fixmap
* 0xfdffb000..0xfe000000 : early ioremap
* 0xf1000000..0xfdffb000 : vmalloc & ioremap
Preemptible hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 4 CPUs
mpic: ISU size: 512, shift: 9, mask: 1ff
mpic: Initializing for 512 sources
clocksource: timebase mult[3bffffec] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
mpic: requesting IPIs...
e500 family performance monitor hardware support registered
Brought up 4 CPUs
devtmpfs: initialized
xor: measuring software checksum speed
8regs : 762.000 MB/sec
8regs_prefetch: 662.000 MB/sec
32regs : 820.000 MB/sec
32regs_prefetch: 727.000 MB/sec
xor: using function: 32regs (820.000 MB/sec)
NET: Registered protocol family 16
Found FSL PCI host bridge at 0x0000000ffe201000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe201000 (primary) ranges:
MEM 0x0000000c20000000..0x0000000c3fffffff -> 0x00000000e0000000
IO 0x0000000ff8010000..0x0000000ff801ffff -> 0x0000000000000000
/pcie@ffe201000: PCICSRBAR @ 0xdf000000
EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe201000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 481 for PCI Err
MPC85xx_edac PCI err registered
PCI: Probing PCI hardware
fsl-pci ffe201000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
pci_bus 0000:00: root bus resource [mem 0xc20000000-0xc3fffffff] (bus address [0xe0000000-0xffffffff])
pci_bus 0000:00: root bus resource [bus 00-ff]
PCIE error(s) detected
PCIE ERR_DR register: 0x80020000
PCIE ERR_CAP_STAT register: 0x80000001
PCIE ERR_CAP_R0 register: 0x00000800
pci 0000:00:00.0: PCI bridge to [bus 01-ff]
PCIE ERR_CAP_R1 register: 0x00000000
PCIE ERR_CAP_R2 register: 0x00000000
PCIE ERR_CAP_R3 register: 0x00000000
PCI: Cannot allocate resource region 0 of device 0000:00:00.0, will remap
pci 0000:00:00.0: BAR 0: can't assign mem (size 0x1000000)
pci 0000:00:00.0: BAR 9: can't assign mem pref (size 0x200000)
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [io 0x0000-0xffff]
pci 0000:00:00.0: bridge window [mem 0xc20000000-0xc3fffffff]
bio: create slab <bio-0> at 0
raid6: int32x1 164 MB/s
raid6: int32x2 227 MB/s
raid6: int32x4 299 MB/s
raid6: int32x8 217 MB/s
raid6: using algorithm int32x4 (299 MB/s)
raid6: using intx1 recovery algorithm
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
Please let me know how to fix the same
I read following mail thread , but couldn't understand what is the problem .
linuxppc-dev - Re: PCIE device errors after linux kernel upgrade | Threaded View
Please post your issue under a new thread -- it doesn't appear to be the same issue. Your log dump doesn't even seem to involve multiple PCIe controllers, as per the thread subject, and your working log shows a 36-bit physical address, so your problem isn't a driver that can't handle such addresses.
When you do create a new thread, be sure to indicate what's actually not working. Those error messages may look scary, but are not likely to be related to whatever problem you're having.