Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

Jump to solution
572 Views
markgreggory
Contributor II

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M? There a project for the TWR-K21d50m in the CW10 folder that I loaded and changed the linker\debug settings to the TWR-k20d50. It compiles and runs but when I plug in the VCP USB cable into a windows machine nothing happens. TWR-k2050d jumpers are in the default setting.

Thanks,

Mark

Labels (1)
Tags (4)
0 Kudos
1 Solution
429 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

View solution in original post

0 Kudos
2 Replies
430 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

0 Kudos
429 Views
markgreggory
Contributor II

Thank you ZhangJennie.

It worked, tight on RAM, but it worked. One problem though. I can't load the CDC drivers on Windows 8. They are not digitally signed. :smileysad:

Mark

0 Kudos