AnsweredAssumed Answered

Re: Help for a beginner with a TWR-K60D100M

Question asked by Zeno Maspoli on Dec 4, 2013
Latest reply on Dec 11, 2013 by Zeno Maspoli
Branched from an earlier discussion

Hi everybody,

 

I just started using this twr, and I'm a brand new user of freescale.

I've downloaded CW for MCU 10.4, and then I've followed the "FLS_MQX_in_CW_10_x" guide

for debug some example project. Now I want to do some easy programs by myself.

For do that the guide use MQX 3.7 Project wizard, my CW created the MQX-lite Project wizard.

If I want to create a MQX (not Lite) project i've to use this PW or there is one

just for MQX ?

Besides when i use MQX-Lite Project Wizard it automatically include Processor Expert without

give me the opportunity to choose as in the MCU PW, so it doesn't create the main.c and create

the ProcessorExpert.c and the Events.c/h. In the example i normaly see project for MQX 3.7 and they work with

main.c and Task.c/h. If i want to work in real time, using the tasks with time delay instead of the interrupt should I

use or not the processor expert ? If not, how can I avoid it ?

thank you

  zeno

Outcomes