Hello Everybody,
I am trying to compile the latest LTIB L3.0.35_4.1.0_130816_source.tar.gz and everything works fine till I reach the gst-fsl-plugins build. As I can see, the compilation is also not throwing any error. The plugin configuration itself seems failing. Can somebody tell me what am I doing wrong? or What is it that I am missing?
Below is the log I get when I try to compile ltib using './ltib'
Processing: gst-fsl-plugins
=============================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/jci/ltib_test/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/jci/ltib_test/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/jci/ltib_test/ltib/tmp' --define '_rpmdir /home/jci/ltib_test/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/jci/ltib_test/ltib/dist/lfs-5.1/fsl-mm/gst-fsl-plugins.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237
+ umask 022
+ cd /home/jci/ltib_test/ltib/rpm/BUILD
+ cd gst-fsl-plugins-3.0.7
++ which pkg-config
+ export 'PKG_CONFIG=/opt/freescale/ltib/usr/bin/pkg-config --static '
+ PKG_CONFIG='/opt/freescale/ltib/usr/bin/pkg-config --static '
++ sed 's,imx\([0-9]*\).*,MX\1,g'
++ echo imx6q
+ PLATFORMSHORTNAME=MX6
+ '[' xMX6 = xMX27 ']'
+ export FBHEADER_PATH=/home/jci/ltib_test/ltib/rootfs/usr/src/linux/include/
+ FBHEADER_PATH=/home/jci/ltib_test/ltib/rootfs/usr/src/linux/include/
++ sed 's,imx\([0-9]*\).*,MX\1,g'
++ echo imx6q
+ ./autogen.sh PLATFORM=MX6
+ aclocal
+ libtoolize --force
libtoolize: putting auxiliary files in `.'.
libtoolize: linking file `./ltmain.sh'
libtoolize: putting macros in AC_CONFIG_MACRO_DIR, `m4'.
libtoolize: linking file `m4/libtool.m4'
libtoolize: linking file `m4/ltoptions.m4'
libtoolize: linking file `m4/ltsugar.m4'
libtoolize: linking file `m4/ltversion.m4'
libtoolize: linking file `m4/lt~obsolete.m4'
+ automake -a
libs/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
libs/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
libs/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
libs/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
libs/Makefile.am:1: its definition is in aclocal's search path.
src/audio/aac_dec/src/Makefile.am:16: Libtool library used but `LIBTOOL' is undefined
src/audio/aac_dec/src/Makefile.am:16: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/aac_dec/src/Makefile.am:16: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/aac_dec/src/Makefile.am:16: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/aac_dec/src/Makefile.am:16: its definition is in aclocal's search path.
src/audio/aacplus_dec/src/Makefile.am:29: Libtool library used but `LIBTOOL' is undefined
src/audio/aacplus_dec/src/Makefile.am:29: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/aacplus_dec/src/Makefile.am:29: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/aacplus_dec/src/Makefile.am:29: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/aacplus_dec/src/Makefile.am:29: its definition is in aclocal's search path.
src/audio/ac3_dec/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined
src/audio/ac3_dec/src/Makefile.am:4: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/ac3_dec/src/Makefile.am:4: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/ac3_dec/src/Makefile.am:4: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/ac3_dec/src/Makefile.am:4: its definition is in aclocal's search path.
src/audio/amr_dec/src/Makefile.am:13: Libtool library used but `LIBTOOL' is undefined
src/audio/amr_dec/src/Makefile.am:13: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/amr_dec/src/Makefile.am:13: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/amr_dec/src/Makefile.am:13: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/amr_dec/src/Makefile.am:13: its definition is in aclocal's search path.
src/audio/amr_enc/src/Makefile.am:13: Libtool library used but `LIBTOOL' is undefined
src/audio/amr_enc/src/Makefile.am:13: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/amr_enc/src/Makefile.am:13: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/amr_enc/src/Makefile.am:13: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/amr_enc/src/Makefile.am:13: its definition is in aclocal's search path.
src/audio/audio_pp/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/audio/audio_pp/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/audio_pp/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/audio_pp/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/audio_pp/src/Makefile.am:1: its definition is in aclocal's search path.
src/audio/beep/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/audio/beep/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/beep/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/beep/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/beep/src/Makefile.am:2: its definition is in aclocal's search path.
src/audio/down_mix/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/audio/down_mix/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/down_mix/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/down_mix/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/down_mix/src/Makefile.am:1: its definition is in aclocal's search path.
src/audio/mp3_dec/src/Makefile.am:20: Libtool library used but `LIBTOOL' is undefined
src/audio/mp3_dec/src/Makefile.am:20: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/mp3_dec/src/Makefile.am:20: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/mp3_dec/src/Makefile.am:20: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/mp3_dec/src/Makefile.am:20: its definition is in aclocal's search path.
src/audio/mp3_enc/src/Makefile.am:19: Libtool library used but `LIBTOOL' is undefined
src/audio/mp3_enc/src/Makefile.am:19: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/mp3_enc/src/Makefile.am:19: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/mp3_enc/src/Makefile.am:19: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/mp3_enc/src/Makefile.am:19: its definition is in aclocal's search path.
src/audio/spdif_rx/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/audio/spdif_rx/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/spdif_rx/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/spdif_rx/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/spdif_rx/src/Makefile.am:1: its definition is in aclocal's search path.
src/audio/spdif_tx/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/audio/spdif_tx/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/spdif_tx/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/spdif_tx/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/spdif_tx/src/Makefile.am:1: its definition is in aclocal's search path.
src/audio/vorbis_dec/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined
src/audio/vorbis_dec/src/Makefile.am:4: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/vorbis_dec/src/Makefile.am:4: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/vorbis_dec/src/Makefile.am:4: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/vorbis_dec/src/Makefile.am:4: its definition is in aclocal's search path.
src/audio/wma10_dec/src/Makefile.am:19: Libtool library used but `LIBTOOL' is undefined
src/audio/wma10_dec/src/Makefile.am:19: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/wma10_dec/src/Makefile.am:19: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/wma10_dec/src/Makefile.am:19: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/wma10_dec/src/Makefile.am:19: its definition is in aclocal's search path.
src/audio/wma8_enc/src/Makefile.am:5: Libtool library used but `LIBTOOL' is undefined
src/audio/wma8_enc/src/Makefile.am:5: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/audio/wma8_enc/src/Makefile.am:5: to `configure.ac' and run `aclocal' and `autoconf' again.
src/audio/wma8_enc/src/Makefile.am:5: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/audio/wma8_enc/src/Makefile.am:5: its definition is in aclocal's search path.
src/misc/i_sink/src/Makefile.am:6: Libtool library used but `LIBTOOL' is undefined
src/misc/i_sink/src/Makefile.am:6: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/misc/i_sink/src/Makefile.am:6: to `configure.ac' and run `aclocal' and `autoconf' again.
src/misc/i_sink/src/Makefile.am:6: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/misc/i_sink/src/Makefile.am:6: its definition is in aclocal's search path.
src/misc/v4l_sink/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/misc/v4l_sink/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/misc/v4l_sink/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/misc/v4l_sink/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/misc/v4l_sink/src/Makefile.am:1: its definition is in aclocal's search path.
src/misc/v4l_source/src/Makefile.am:7: Libtool library used but `LIBTOOL' is undefined
src/misc/v4l_source/src/Makefile.am:7: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/misc/v4l_source/src/Makefile.am:7: to `configure.ac' and run `aclocal' and `autoconf' again.
src/misc/v4l_source/src/Makefile.am:7: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/misc/v4l_source/src/Makefile.am:7: its definition is in aclocal's search path.
src/parser/aiur/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/parser/aiur/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/parser/aiur/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/parser/aiur/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/parser/aiur/src/Makefile.am:2: its definition is in aclocal's search path.
src/video/deinterlace/src/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
src/video/deinterlace/src/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/deinterlace/src/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/deinterlace/src/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/deinterlace/src/Makefile.am:1: its definition is in aclocal's search path.
src/video/h264_dec/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined
src/video/h264_dec/src/Makefile.am:21: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/h264_dec/src/Makefile.am:21: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/h264_dec/src/Makefile.am:21: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/h264_dec/src/Makefile.am:21: its definition is in aclocal's search path.
src/video/ipu_csc/src/Makefile.am:6: Libtool library used but `LIBTOOL' is undefined
src/video/ipu_csc/src/Makefile.am:6: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/ipu_csc/src/Makefile.am:6: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/ipu_csc/src/Makefile.am:6: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/ipu_csc/src/Makefile.am:6: its definition is in aclocal's search path.
src/video/mpeg2_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/video/mpeg2_dec/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/mpeg2_dec/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/mpeg2_dec/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/mpeg2_dec/src/Makefile.am:2: its definition is in aclocal's search path.
src/video/mpeg4asp_dec/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined
src/video/mpeg4asp_dec/src/Makefile.am:21: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/mpeg4asp_dec/src/Makefile.am:21: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/mpeg4asp_dec/src/Makefile.am:21: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/mpeg4asp_dec/src/Makefile.am:21: its definition is in aclocal's search path.
src/video/vpu/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/video/vpu/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/vpu/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/vpu/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/vpu/src/Makefile.am:2: its definition is in aclocal's search path.
src/video/vpu_dec.full/src/Makefile.am:21: Libtool library used but `LIBTOOL' is undefined
src/video/vpu_dec.full/src/Makefile.am:21: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/vpu_dec.full/src/Makefile.am:21: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/vpu_dec.full/src/Makefile.am:21: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/vpu_dec.full/src/Makefile.am:21: its definition is in aclocal's search path.
src/video/vpu_enc/src/Makefile.am:4: Libtool library used but `LIBTOOL' is undefined
src/video/vpu_enc/src/Makefile.am:4: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/vpu_enc/src/Makefile.am:4: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/vpu_enc/src/Makefile.am:4: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/vpu_enc/src/Makefile.am:4: its definition is in aclocal's search path.
src/video/wmv9mp_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/video/wmv9mp_dec/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/wmv9mp_dec/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/wmv9mp_dec/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/wmv9mp_dec/src/Makefile.am:2: its definition is in aclocal's search path.
src/video/wmv_dec/src/Makefile.am:2: Libtool library used but `LIBTOOL' is undefined
src/video/wmv_dec/src/Makefile.am:2: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
src/video/wmv_dec/src/Makefile.am:2: to `configure.ac' and run `aclocal' and `autoconf' again.
src/video/wmv_dec/src/Makefile.am:2: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
src/video/wmv_dec/src/Makefile.am:2: its definition is in aclocal's search path.
tools/gplay/Makefile.am:1: Libtool library used but `LIBTOOL' is undefined
tools/gplay/Makefile.am:1: The usual way to define `LIBTOOL' is to add `AC_PROG_LIBTOOL'
tools/gplay/Makefile.am:1: to `configure.ac' and run `aclocal' and `autoconf' again.
tools/gplay/Makefile.am:1: If `AC_PROG_LIBTOOL' is in `configure.ac', make sure
tools/gplay/Makefile.am:1: its definition is in aclocal's search path.
Makefile.am:972: `%'-style pattern rules are a GNU make extension
+ exit 1
error: Bad exit status from /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237 (%build)
RPM build errors:
Bad exit status from /home/jci/ltib_test/ltib/tmp/rpm-tmp.25237 (%build)
Build time for gst-fsl-plugins: 12 seconds
Failed building gst-fsl-plugins
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Mon Nov 25 10:50:06 2013
Ended: Mon Nov 25 10:50:55 2013
Elapsed: 49 seconds
These packages failed to build:
gst-fsl-plugins
Build Failed
Exiting on error or interrupt
Solved! Go to Solution.
Hi,
Solved the issue. libtool was missing from my system. Had to install it and got everything working again
$ sudo apt-get install libtool
did the trick.
Thanks & Regards,
- Ketan
Hi,
Solved the issue. libtool was missing from my system. Had to install it and got everything working again
$ sudo apt-get install libtool
did the trick.
Thanks & Regards,
- Ketan
Hi Ketan,
I see you have solved your problem, would you please click Corect Answer/Helpful Answer. We would assume your issue/question got answered if no response from you in 3 days and close the DI. Thanks a lot.
Any other questions will be welcome~~
Best Regards
Dan