AnsweredAssumed Answered

USBDM with glibc older than 2.14 on Debian Stable

Question asked by B Thomas on Nov 23, 2013
Latest reply on Nov 23, 2013 by pgo

I just downloaded the USBDM deb package. It installed cleaning on Debian/Stable (Wheezy). However in trying to run any application I get the following error

 

HCS08_FlashProgrammer: /lib/x86_64-linux-gnu/libc.so.6: version `GLIBC_2.14' not found (required by HCS08_FlashProgrammer)

HCS08_FlashProgrammer: /lib/x86_64-linux-gnu/libc.so.6: version `GLIBC_2.14' not found (required by /usr/lib/x86_64-linux-gnu/usbdm/libusbdm.so.4)

 

This is because usbdm was compiled with GLIBC 2.14 but Debian Stable only provides GLIBC 2.13. If it were compiled with an older version

version of GLIBC (such as that available on Ubuntu Long Term Stable or Debian Stable) it will execute without problems with the newer

version but not the other way round.

 

However I am unable to find instructions on how to compile this software on a GNU/Linux system. Is this possible ? Could you please advice ?

At present I only need the HCS08_FlashProgrammer and perphas the Eclipse Plugin.

 

Sincerely

B Thomas

Outcomes