Hi All,
My customer is using 30MHZ crystal in their target board and want to use UART0 for communication, I have downloaded Kinetis_120MZ_SC sample code and in the hello_Word program and in the Trw-K60F120M.h there is below settings, If I want to change the crystal value CLK1_FREQ_HZ to 30000000 & TERM_PORT to UART0 does it support.
Please let me know if other settings need to be configured
#define CLK1_FREQ_HZ 12000000
#define CLK1_TYPE CRYSTAL
/* Serial Port Info */
#define TERM_PORT UART5_BASE_PTR
Regards
Mithun
Hi all,
I'm also looking for changing my project from MK60FN1M0 to MK60FX512.
But is there a real difference between the two target?
Because my project works on a MK60FX512 even if it's designed for a MK60FN1M0.
Can I have some trouble without changing the coonfiguration?
Regards,
Guillaume
Hi Zhe Tian,
Thanks actually in my customer target board they are using MK60FX512 and the Kinetis_120MHZ_SC sample code are based on MK60FN1M0 please help me how can I port them/change them to work for MK60FX512.
Regards
Mithun
Hi, Mithun
Yes, you can change it. The reminder is please pay attention to baud rate changing. Thanks.
Best Regards
Paul