where is sdhci_esdhc_imx_driver_init ???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is sdhci_esdhc_imx_driver_init ???

Jump to solution
863 Views
EdSutter
Senior Contributor II

This one really has me stumped...

I'm trying to trace through some of the kernel code to understand why I can't access eMMC.

I put a dump_stack() call at the top of the function sdhci_add_host() (in drivers/mmc/host/sdhci.c kernel=3.11.4).

When I boot up, I get a stack trace that looks something like this...

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.11.4 #22

Backtrace:

[<80011ddc>] (dump_backtrace+0x0/0x10c) from [<80011f78>] (show_stack+0x18/0x1c)

r6:bfba82c0 r5:bfba82c0 r4:00000000 r3:00000000

[<80011f60>] (show_stack+0x0/0x1c) from [<80548398>] (dump_stack+0x80/0x9c)

[<80548318>] (dump_stack+0x0/0x9c) from [<8040d388>] (sdhci_add_host+0x24/0xbb4)

r4:bfb21d10 r3:00000000

[<8040d364>] (sdhci_add_host+0x0/0xbb4) from [<8040ef4c>] (sdhci_esdhc_imx_probe+0x28c/0x560)

[<8040ecc0>] (sdhci_esdhc_imx_probe+0x0/0x560) from [<802f8740>] (platform_drv_probe+0x20/0x24)

r8:80705e38 r7:80756c38 r6:00000000 r5:bf981e10 r4:807b2178

[<802f8720>] (platform_drv_probe+0x0/0x24) from [<802f739c>] (driver_probe_device+0x10c/0x224)

[<802f7290>] (driver_probe_device+0x0/0x224) from [<802f7548>] (__driver_attach+0x94/0x98)

r7:00000000 r6:bf981e44 r5:80756c38 r4:bf981e10

[<802f74b4>] (__driver_attach+0x0/0x98) from [<802f58a8>] (bus_for_each_dev+0x5c/0x90)

r6:802f74b4 r5:80756c38 r4:00000000 r3:bf83c85c

[<802f584c>] (bus_for_each_dev+0x0/0x90) from [<802f6e90>] (driver_attach+0x20/0x28)

r6:80746068 r5:bfb21c80 r4:80756c38

[<802f6e70>] (driver_attach+0x0/0x28) from [<802f6a08>] (bus_add_driver+0xdc/0x238)

[<802f692c>] (bus_add_driver+0x0/0x238) from [<802f7a6c>] (driver_register+0x80/0x154)

r8:80705e38 r7:806e746c r6:80762800 r5:00000006 r4:80756c38

[<802f79ec>] (driver_register+0x0/0x154) from [<802f8964>] (__platform_driver_register+0x50/0x64)

[<802f8914>] (__platform_driver_register+0x0/0x64) from [<80705e50>] (sdhci_esdhc_imx_driver_init+0x18/0x20)

[<80705e38>] (sdhci_esdhc_imx_driver_init+0x0/0x20) from [<80008798>] (do_one_initcall+0xf4/0x154)

[<800086a4>] (do_one_initcall+0x0/0x154) from [<806e7c24>] (kernel_init_freeable+0x104/0x1d0)

[<806e7b20>] (kernel_init_freeable+0x0/0x1d0) from [<805441f8>] (kernel_init+0x10/0xec)

[<805441e8>] (kernel_init+0x0/0xec) from [<8000e8b8>] (ret_from_fork+0x14/0x3c)

r4:00000000 r3:ffffffff                                                

Referring to the stack trace, I see that the function sdhci_esdhc_imx_driver_init is called, so I tried to look at that code in the kernel...

Its not there; yet it does show up in the System.map (and several other .o) files.  Then I thought maybe my browser wasn't showing

me the function, so I did a brute force find/grep on the whole tree...

First I did it on the tree that I had built and it showed me that the function name was in several .o files and also in the System.map file...

find . -type f -exec grep -l sdhci_esdhc_imx_driver_init {} \;

./drivers/built-in.o

./drivers/mmc/host/built-in.o

./drivers/mmc/host/sdhci-esdhc-imx.o

./drivers/mmc/built-in.o

./System.map

./.tmp_vmlinux1

./.tmp_System.map

./vmlinux.o

./.tmp_vmlinux2

./vmlinux

then I did it on a clean source tree and it came back empty.

Whats up with that?  How can the function exist symbolically but not be in the source code somewhere?

Ed

Labels (1)
0 Kudos
1 Solution
641 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Sutter

     The sdhci_esdhc_imx_driver_init is wrapped in module_platform_driver(sdhci_esdhc_imx_driver); of drivers/mmc/host/sdhci-esdhc-imx.c, see below:

include/linux/platform_device.h:

208 #define module_platform_driver(__platform_driver) \

209         module_driver(__platform_driver, platform_driver_register, \

210                         platform_driver_unregister)

include/linux/device.h:

1138 #define module_driver(__driver, __register, __unregister, ...) \

1139 static int __init __driver##_init(void) \

1140 { \    

1141         return __register(&(__driver) , ##__VA_ARGS__); \

1142 } \

1143 module_init(__driver##_init); \

View solution in original post

0 Kudos
2 Replies
642 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Sutter

     The sdhci_esdhc_imx_driver_init is wrapped in module_platform_driver(sdhci_esdhc_imx_driver); of drivers/mmc/host/sdhci-esdhc-imx.c, see below:

include/linux/platform_device.h:

208 #define module_platform_driver(__platform_driver) \

209         module_driver(__platform_driver, platform_driver_register, \

210                         platform_driver_unregister)

include/linux/device.h:

1138 #define module_driver(__driver, __register, __unregister, ...) \

1139 static int __init __driver##_init(void) \

1140 { \    

1141         return __register(&(__driver) , ##__VA_ARGS__); \

1142 } \

1143 module_init(__driver##_init); \

0 Kudos
641 Views
EdSutter
Senior Contributor II

Ok, i see.

Thanks!

0 Kudos