How to set VF3x core clock to 266 MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set VF3x core clock to 266 MHz?

Jump to solution
650 Views
MehmetAliIpin
Contributor V

Dear Sir/Madam,

I have a protoype board for VF3x. I am using DS-5 and MQX to test it. Since MQX is prepared for tower kit, the core clock is set to 399 MHz in clocks.init() in init_hw.c file, as below:

    // wait to lock pll

    while ((Anadig_PLL_LOCK & PLL_LOCKS) != PLL_LOCKS);

    // ARM_CLK: SYS_CLK/1 = 396Mhz

    // BUS_CLK: ARM_CLK/3 = 132Mhz

    // IGP_CLK: BUS_CLK/2 = 66Mhz

    // AUDIO_DIV:  73Mhz ??

    CCM_CACRR = CCM_CACRR_ARM_CLK_DIV(0) | CCM_CACRR_BUS_CLK_DIV(2) | CCM_CACRR_IPG_CLK_DIV(1) | CCM_CACRR_PLL4_CLK_DIV(7);

There are definitions for the CCM_CACRR_ARM_CLK_DIV() in MVF50GS10MK50.h file as:

#define CCM_CACRR_ARM_CLK_DIV_MASK               0x7u

#define CCM_CACRR_ARM_CLK_DIV_SHIFT              0

#define CCM_CACRR_ARM_CLK_DIV(x)                 (((uint32_t)(((uint32_t)(x))<<CCM_CACRR_ARM_CLK_DIV_SHIFT))&CCM_CACRR_ARM_CLK_DIV_MASK)

But it is not easy to reach a result from this line for me. How can I set the core frequency to 266 MHz? ( I guess it is the maximum frequency for VF3x)

Thanks and best regards.

Mehmet Ali Ipin

Labels (4)
0 Kudos
1 Solution
400 Views
juangutierrez
NXP Employee
NXP Employee

Nothe that Im refering to code in twrvf65gs10 but it should be very similar for vf3 or maybe identical

In clocks_init you should have some seeting for the CCM_CCSR like below:

CCM_CCSR = 0x0003FF24;  

which set (among other things)

       CCM_CCSR[PLL1_PFD_CLK_SEL] = 0x3  ----> PLL1 uses PLL1_PFD3

       CCM_CCSR[SYS_CLK_SEL] = 0x4 ----> use PLL1_PFD

The Anadig_PLL_PFD_528 might NOT be set, because using the default RESET values

From Reference Manual the reset value for pfd3_frac is:

    Anadig_PLL_PFD_528[PFD3_FRAC] = 0x18 = d24

This is setting the resulting freq = 528 * 18/24 = 396 MHz, through the next path

396Mhz.png

For getting the 266MHz Frequency at PLL1_PFD3 you need to tweak the value of Anadig_PLL_PFD_528[PFD3_FRAC] close to 266MHz is

Anadig_PLL_PFD_528[PFD3_FRAC] = d36 = 0x24

PLL1_PFD3_freq = 528 * 18 / 36 = 264 Mhz

SYS_CLK = PLL1_PFD3_freq / ARM_CLK_DIV = 264/1 = 264Mhz

You can try to check if there is a better way to get a closer value to 266Mhz.

You need to tweak different values like Anadig_PLL_PFD_528[PFD3_FRAC], Anadig_PLL1_CTRL[DIV_SELECT], CCM_CACRR[ARM_CLK_DIV], etc.

You can try setting a smaller value in the PFD3_FRAC, so PLL1_PFD3 output is a higher frequency and set a higher divisor value in CCM_CACRR[ARM_CLK_DIV].

View solution in original post

0 Kudos
2 Replies
401 Views
juangutierrez
NXP Employee
NXP Employee

Nothe that Im refering to code in twrvf65gs10 but it should be very similar for vf3 or maybe identical

In clocks_init you should have some seeting for the CCM_CCSR like below:

CCM_CCSR = 0x0003FF24;  

which set (among other things)

       CCM_CCSR[PLL1_PFD_CLK_SEL] = 0x3  ----> PLL1 uses PLL1_PFD3

       CCM_CCSR[SYS_CLK_SEL] = 0x4 ----> use PLL1_PFD

The Anadig_PLL_PFD_528 might NOT be set, because using the default RESET values

From Reference Manual the reset value for pfd3_frac is:

    Anadig_PLL_PFD_528[PFD3_FRAC] = 0x18 = d24

This is setting the resulting freq = 528 * 18/24 = 396 MHz, through the next path

396Mhz.png

For getting the 266MHz Frequency at PLL1_PFD3 you need to tweak the value of Anadig_PLL_PFD_528[PFD3_FRAC] close to 266MHz is

Anadig_PLL_PFD_528[PFD3_FRAC] = d36 = 0x24

PLL1_PFD3_freq = 528 * 18 / 36 = 264 Mhz

SYS_CLK = PLL1_PFD3_freq / ARM_CLK_DIV = 264/1 = 264Mhz

You can try to check if there is a better way to get a closer value to 266Mhz.

You need to tweak different values like Anadig_PLL_PFD_528[PFD3_FRAC], Anadig_PLL1_CTRL[DIV_SELECT], CCM_CACRR[ARM_CLK_DIV], etc.

You can try setting a smaller value in the PFD3_FRAC, so PLL1_PFD3 output is a higher frequency and set a higher divisor value in CCM_CACRR[ARM_CLK_DIV].

0 Kudos
400 Views
MehmetAliIpin
Contributor V

Dear Rosas,

Thank you so much for your detailed information.

with my best regards.

0 Kudos