AnsweredAssumed Answered

MX53 FlexCAN can not received remote request frame?

Question asked by Frank Chen on Nov 14, 2013
Latest reply on Feb 6, 2015 by alejandrolozano

Hi, I connected two MX53 boards to perform CAN test. I ran cansend on one board, and candump on the other. For standard or extended frames the test worked fine. But when test remote request frames, the cansend seems OK, but candump didn't receive anything.

 

The commands are as follows:

Board A:

# cansend can0 -i 25 -r -v

Board B:

# candump

 

The BSP I used is MX53 Android R10.3.

 

Any comment is welcome. Thanks!

Outcomes