AnsweredAssumed Answered

sabre SD eMMC

Question asked by Niklas Molin on Nov 14, 2013
Latest reply on Nov 15, 2013 by Leonardo Sandoval Gonzalez

Hi.

 

I just received a Sabre SD board and trying to access the 8GB eMMC chip (I think it is connected on SD4).

First I notice I can't boot from the eMMC, only from the SD card slots.

When I boot on the SD card, I can't find the eMMC.

I'm pretty sure it is a small detail I have missed.

I have been trying the Linux image that was provided with the board (not sure what environment they used to build that one) and I have also tried the image I build in the Yocto environment.

But I can't see the eMMC.

My question is what device (/dev/...) I need to mount to access that chip?

When I start u-boot only I can see the eMMC chip.

 

Thanks,

Niklas

Outcomes