Just to add a little bit to Zhang's explanation, several legacy BSPs were retired in MQX 4.0.0 in order to focus on newer processors and features. These boards are listed in the MQX release notes under Version 4.0.0 changes, and as pointed out above, MQX 3.8.1 is still available for free download if you need access to these BSPs.
The following board support packages were removed from the release and will be supported only as a part of MQX 3.8.1 version maintenance.
o TWR-MCF51AG, TWR-MCF51CN, TWR-MCF51JE, TWR-MCF51MM, TWR-MCF51QM, DEMOEM, DEMOAC, EVB51JM128, M5208EVB, M52223EVB, M52233DEMO, M52235EVB, M52277EVB, M53015EVB, M5329EVB, M54455EVB and MPC8308RDB
-Anthony
on my side, my mqx4.0.2 doesn't include 51cn bsp, but mqx3.8.1 includes it. here is its download link:
Just to add a little bit to Zhang's explanation, several legacy BSPs were retired in MQX 4.0.0 in order to focus on newer processors and features. These boards are listed in the MQX release notes under Version 4.0.0 changes, and as pointed out above, MQX 3.8.1 is still available for free download if you need access to these BSPs.
The following board support packages were removed from the release and will be supported only as a part of MQX 3.8.1 version maintenance.
o TWR-MCF51AG, TWR-MCF51CN, TWR-MCF51JE, TWR-MCF51MM, TWR-MCF51QM, DEMOEM, DEMOAC, EVB51JM128, M5208EVB, M52223EVB, M52233DEMO, M52235EVB, M52277EVB, M53015EVB, M5329EVB, M54455EVB and MPC8308RDB
-Anthony
btw, I did a live chat trying to get help. He suggested getting FreeRTOS instead! Not that it's really free, since you have to pay for the documentation about how to use it.
can you please specify why need to pay for the document?
I didn't see where they had documentation available except in their store where they want $30 for a PDF of the reference manual (here's the link)
i never use freeRTOS but i just perform search in google i find some other resource:
http://www.freertos.org/RTOS.html
did you ever check them.
Thanks! Now all I have to do is figure out how to get at it.