Hi everybody,
So, I have decided to make a new project using the MC9S08PA4 to replace a MC9S08SH8 in a project that a I have done some time ago, until then everything was ok. The problem begins when I have started to test the new PA4 that I have ordered (samples). With this sample parts, I simply can't debug or run the code that I have made, even a simple led blink code (as below) does not work as it should...
#include <hidef.h> /* for EnableInterrupts macro */ #include "derivative.h" /* include peripheral declarations */ void main(void) { unsigned int Loop = 0; volatile unsigned char ST = 0; ST = SYS_SRS; SYS_SOPT1 = 0b00001100; // RESET and BKGD active WDOG_CS1 = 0; // disable WDT PORT_PTAOE = 0b00000001; PORT_PTAIE = 0b11111110; PORT_PTAPE = 0b11001110; PORT_PTAD_PTAD0 = 0; for(;;) { PORT_PTAD_PTAD0 = 1; for(Loop=0;Loop<50000;Loop++); PORT_PTAD_PTAD0 = 0; for(Loop=0;Loop<50000;Loop++); } }
The LED is connected on PTA0 (pin 20) with a 1K resistor to GND.
Everytime that I need to program the microcontroller (on run or debug) I must power off and power on the power supply.
When I try to debug, I can run the program step by step until line 23, after this point the program lost itself and I get the message "Target request failed: HC/RS/S12Z GDI Protocol Adapter : Stop failed. Non Fatal Error.".
When I try to run the code the LED stays lit forever.
I'm have tested this code with the CW 10.4 and CW 10.5 using the CYCLONE PRO via USB to program the microcontroller and the results are the same.
Any help is welcome!
Thanks!
Solved! Go to Solution.
Try this code to disable the WDT:
/Unlocking Watchdog Registers
WDOG_CNT = 0xC520; // write 0xC520 to the 1st unlock word
WDOG_CNT = 0xD928; // write 0xD928 to the 2nd unlock word
//Disable Watchdog
WDOG_CS1 = 0; // disable Watchdog
WDOG_CS2 = 0;
WDOG_TOVAL = 0xFFFF;
WDOG_WIN = 0x0000;
Mike
hi jonny
i have got similar problems with mc9s08pt32 . i think there is a problem with disabling wdt. i can not disable wdt. probably wdt resets your system during step by step working.
and while i programming each time it asks me to power up the system.
and while running i can not stop the code clicking the stop button on the screen.
regards
Try this code to disable the WDT:
/Unlocking Watchdog Registers
WDOG_CNT = 0xC520; // write 0xC520 to the 1st unlock word
WDOG_CNT = 0xD928; // write 0xD928 to the 2nd unlock word
//Disable Watchdog
WDOG_CS1 = 0; // disable Watchdog
WDOG_CS2 = 0;
WDOG_TOVAL = 0xFFFF;
WDOG_WIN = 0x0000;
Mike
Hello,
I had the same Problem on an S08PT60. I use Assembly language and according to Mike´s solution
I want to post my assembly code here. Thank you Mike, it works for me too!
After Startup:
_Startup:
LDHX #RAMEnd+1 ; initialize the stack pointer
TXS
SEI ; disable interrupts
lda #%00001100
sta SYS_SOPT1
jsr Watchdog_disable
bra mainLoop
mainLoop:
bra mainLoop
Watchdog_disable:
psha
ldhx #$C520
sthx WDOG_CNT
ldhx #$D928
sthx WDOG_CNT
lda #$00
sta WDOG_CS1
lda #$00
sta WDOG_CS2
ldhx #$FFFF
sthx WDOG_TOVAL
ldhx #$0000
sthx WDOG_WIN
pula
rts
Sorry for the delay, michaelsteffenfae, thanks for your answer, now it worked very well!
Thanks!
thanks michael
i missed that fact at the features of wdt. i looked at register definitions directly. we always try to make development quickly. but freescale must put a note in the register definitions that these resisters should be unlocked before altering them.
regards
yuksel celik, that's a good idea, this could help more people that are beginning working with PA/PT families.
Thanks!