AnsweredAssumed Answered

iMX6 screen tearing artifacts when using Linux/X11/Chromium

Question asked by Gabriel Liseanu on Nov 12, 2013
Latest reply on Jan 11, 2014 by Pratik Pawar

Hello,

 

when using Linux/X11/Chrome on a SABRE Dual Lite  board, screen tearing artifacts are encountered within the broswer. Following setup is used:

 

- Yocto Release 1.5, including

 

- Linux imx6dlsabresd 3.0.35-4.1.0+yocto+gbdde708 ( only one cpu activated )

- X.Org X Server 1.14.0

- Chrome Version 32.0.1664.3 ( 227606 ), with all GPU acceleration options enabled

 

When the Video Tearing test - YouTube is displayed inside the browser,  tearing artifacts are visible. Tearing artifacts are also visible when swiping html5 pages.

 

If the same URL ( the YouTube tearing video )  is displayed on the SABRE Dual Lite board using an Android 4.2.2 image + Chrome 29.0.1547.59 no tearing artifacts are visible.

 

Is this behaviour known ? Are there any hints available, regarding the configuration of the subsystems preventing the tearing artifacts mentioned above ?

 

Any help would be highly appreciated.

 

Kind regards,

Gabriel.

Outcomes