VF5xx/about VDDA33_AFE, VDD12_AFE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF5xx/about VDDA33_AFE, VDD12_AFE

Jump to solution
498 Views
soichiyamamoto
Contributor V

Hi, Dose VDDA33_AFE, VDD12_AFE use for Video ADC? I not use Video ADC. For reasons of it, do I not need to use VDDA33_AFE, VDD12_AFE? Best regards, soichi yamamoto

Labels (1)
0 Kudos
1 Solution
364 Views
timesyssupport
Senior Contributor II

Hello Soichi-san,

After reviewing the datasheet for the VF6xx, it appears that VDDA33_AFE and VDD12_AFE are only used for Video ADC, so you should not need to use these if you are not using Video ADC.

Regards,

Timesys Support

View solution in original post

0 Kudos
2 Replies
364 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport are you available  to help on this case?

0 Kudos
365 Views
timesyssupport
Senior Contributor II

Hello Soichi-san,

After reviewing the datasheet for the VF6xx, it appears that VDDA33_AFE and VDD12_AFE are only used for Video ADC, so you should not need to use these if you are not using Video ADC.

Regards,

Timesys Support

0 Kudos