L3.0.35_4.0.0_130424_images_MX6 -reg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L3.0.35_4.0.0_130424_images_MX6 -reg

686 Views
bottleneck
Contributor II

Hi,

Currently working on SABRESDB board,I am trying to load latest kernel but

still unsuccessful.

I saw pre-compiled images L3.0.35_4.0.0_130424_images_MX6, I am trying to

use the latest

boot loader by loading it to RAM and execute it in RAM itself by removing

SD Card.But I have

doubt to which address I need to load u-boot binary

(u-boot-mx6q-sabresd.bin).

Next I would like to know the pre-compiled uImage is for NFS or TFTP boot.

I tried both methods

but unsuccessful, currently on the SD card U-Boot 2009.08-00602-g3f71ed9

and Android Image

with Linux 3.0.35 version is available.In the following addresses uImage

and rootfs is loaded using

TFTP.

0x108000000 and 0x14000000

For the NFS, I installed nfs-kernel server and then updated /etc/exports

and mounted the root file

system in /tftpboot/nfsroot.

In TFTP case, it shows corrupted ramdisk and in NFS it keeps rebooting

without mounting

the file system.

Please guide me if I am wrong anywhere.

Thanks

Umamahesh Y V

0 Kudos
1 Reply

264 Views
Yuri
NXP Employee
NXP Employee

You may use the recent BSP (L3.0.35_4.1.0) from the Web.

< https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_DEMO_IMAGE_BSP&appType=license&locat... >

< https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_ER_SOURCE_BSP&appType=license&locati... >

  Chapter 7 (Downloading Images by Bootloader or NFS) and section 3.3 (Setting
rootfs for NFS) of the Linux User’s Guide (“i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf”)
describes how to configure and use NFS options.

As for U-boot load address, please apply to MFG configuration (ucl2.xml) :
load address is 0x10800000.

0 Kudos