[Q5]When resuming from suspend,the activesync runs many times and reports erro,even it does not connect with PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Q5]When resuming from suspend,the activesync runs many times and reports erro,even it does not connect with PC

620 Views
johnphy
Contributor I

Hi,    Thanks for your attenion.    We are using  I.MX53 running WEC7. The registery storage is "Hive-based Registry" and the file system is  "RAM and ROM file system".

1,Connect the USB slave port to PC, and the activesync funtion runs good; If we do not use the activesync function , the device can be seen as a "sd memory card" on PC and has no problem;

2,Connect a USB mouse to the device USB HOST port , and it works well;

3, Set the device to suspend mode,

4, When the device resumes from suspend state, the USB mouse works well and has no problem.

5, When the device resumes from suspend state, it starts activesync many times and reports erro, even it does not connect with PC.     Why      and    how   can we stop it?


Here are the debug messages the device reports :

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:037D0026 TID:03AE0026 Error from RasDial 608 0

PID:037D0026 TID:03AE0026 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:09AB0012 TID:09AD0012 Error from RasDial 608 0

PID:09AB0012 TID:09AD0012 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:09810046 TID:09B10032 Error from RasDial 608 0

PID:09810046 TID:09B10032 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:09DB0072 TID:09DD0072 Error from RasDial 608 0

PID:09DB0072 TID:09DD0072 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:08F3009A TID:08F5009A Error from RasDial 608 0

PID:08F3009A TID:08F5009A Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:084C00A2 TID:084D00A2 Error from RasDial 608 0

PID:084C00A2 TID:084D00A2 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:08A600FA TID:08AB00FA Error from RasDial 608 0

PID:08A600FA TID:08AB00FA Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:0819012E TID:081B012E Error from RasDial 608 0

PID:0819012E TID:081B012E Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:092E0152 TID:09300152 Error from RasDial 608 0

PID:092E0152 TID:09300152 Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [1] [Dialer Start]

PID:09080166 TID:09D0015E Error from RasDial 608 0

PID:09080166 TID:09D0015E Posting WM_NETCONNECT(FALSE) message, ErrorCode = 608(0x260)

PID:00400002 TID:05600006 AUTORAS:: Dialer notifies: [2] [Dialer Terminate]

Labels (1)
0 Kudos
1 Reply

411 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

I saw this behavior before on my side,

-    When OTG as pure client is selected, OTG is detecting as client. I am able to use Active sync.

-    When OTG as pure host is selected, OTG is detecting as host. I am able to connect mouse.

-    When OTG full function is selected, only OTG client is working. OTG as host is not working. Run time it is not switching between OTG client and host.

I had to use the full-function OTG driver as a Host and connect some device to it, to made it workAlso please check that the ID pin of the USB OTG port tied to ground?

Hope this helps

0 Kudos