AnsweredAssumed Answered

CW? - S08GT60 MC13192 - ADC conversion sent over SMAC Where do I start??

Question asked by Eduardo Estigoni on Aug 1, 2007
Latest reply on Aug 1, 2007 by Eduardo Estigoni
Hi Guys,

I have just started to use codewarrior and need some advice...
I have 2 boards with MC9S08GT60 mcu and  MC13192 transc on. I will be receiving my USBMULTILINK in few days and I wanna get started using the simulation first.

In the end, I will need to write a code to collect samples from the AD using the mcu MC9S08GT60 on one of the boards and transmit to the other.

So, I was wondering if there is a template to start working on.
I've downloaded the BeeKit, and I created some projects to export to CodeWarrior. But I didn't really get the idea yet... Is it the best way to go? Or should I start doing something with the AD first and then try to add the SMAC stuff?

Cheers,

Ed.

--
Alban Edit: FSL Part Number must figure in Message Subject line.





Message Edited by Alban on 2007-08-01 11:38 AM

Outcomes