When running bare metal code on the i. MX6 Solo I always get a software interrupt. UBOOT tells me the reset cause is WDOG. How do I fix this?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When running bare metal code on the i. MX6 Solo I always get a software interrupt. UBOOT tells me the reset cause is WDOG. How do I fix this?

1,488 Views
kyleengstrom
Contributor I

This is how I reset the watchdog timer in my baremetal code.

Freescale i.MX6SOLO rev1.1

static void watchdog_reset(void)

       {

    watchdog_reg_p base = (watchdog_reg_p) WDOG1_BASE_ADDR;

    /* Init Watchdog */

    base->wcr = WCR_WDA | WCR_SRS | WCR_WT | WCR_WDBG;

    /*enable watchdog */

    base->wcr |= WCR_WDE;

    base->wsr = 0x5555;

    base->wsr = 0xAAAA;

    }

Uboot gives me this when I try and run my code.

U-Boot > fatload usb 0:1 0x12000000 testme.axf

fatload usb 0:1 0x12000000 testme.axf

reading testme.axf

95376 bytes read in 57 ms (1.6 MiB/s)

U-Boot > bootelf

bootelf

## Starting application at 0x00900000 ...

software interrupt

pc : [<00903a28>]   lr : [<00903a28>]

sp : 0093efe0  ip : 0093e010 fp : 00904a60

r10: 00904a60  r9 : 2f359f38 r8 : 2f35b9a0

r7 : 00904a4f  r6 : 00000000 r5 : 00000000  r4 : 00000000

r3 : 00000000  r2 : 0093e000 r1 : 00000000  r0 : 00000010

Flags: nzCv  IRQs off  FIQs off  Mode SVC_32

Resetting CPU ...

resetting ...

U-Boot 2013.10-rc4-00124-g2c62998 (Oct 14 2013 - 14:45:57)

CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

Reset cause: WDOG

I can see that the program runs till it hits location 903a28 before being stopped with a software interrupt. I believe that uboot turns off the watchdog timer on the i.MX6. Does anything look weird here? How should I move forward debugging this? We are trying to run bare metal applications on the i.MX6 Solo without using the debugger tools. What is the best way to accomplish this? Uboot seems to work fine we just keep getting this software interrupt.

Oh and the I'm using

U-Boot 2013.10-rc4-00124-g2c62998 (Oct 14 2013 - 14:45:57)

Thank you so much for any help!

Best regards.

Labels (2)
0 Kudos
3 Replies

589 Views
Yuri
NXP Employee
NXP Employee

1.

Watchdog Enable bit is a write one once only bit. It is not possible to clear this bit by a software write,

once the bit is set.


2.

"Once the WDOG is activated, it must be serviced by the software on a periodic basis. If

servicing does not take place, the timer times out. Upon timeout, the WDOG asserts the

internal system reset signal".

So, it is needed to provide codes to clear WDOG counters periodically.

0 Kudos

589 Views
kyleengstrom
Contributor I

Still waiting on a reply. Why does it say "This question is Assumed Answered." This question is most definitely NOT answered.

0 Kudos

589 Views
kyleengstrom
Contributor I

Hmm, thanks for the quick reply. We use the function posted above to reset the WDOG. We call it every time our loop runs which is constantly. Will this not reset the WDOG timer? (See above)

0 Kudos